Other Parts Discussed in Thread: OMAP-L138
Hi there
I am trying to run AISgen (Version 1.7c) on the command line, the code is for the ARM part of an OMAP-L138. I followed the documentation (sprab41b) to create a config file (see below), but when I try to run AISgen with this config from the command line, it doesn't create the output file.
The AISgen log file gives the following, a little vague error message:
***Loaded configuration from file AISConfig.cfg
***One or more parameter error must be corrected.
This problem only occurs when I try to use the command line ith the -cfg option. When I start AISgen without it and then use File->Load Configuration to load the very same config, no error occurs and the output file is created.
Yours,
Björn.
---Bootloader.cfg---
Boot Mode=SPI1 Flash
Boot Speed=1
Flash Width=0
Flash Timing=3ffffffc
Configure Peripheral=True
Configure PLL0=False
Configure SDRAM=False
Configure PLL1=False
Configure DDR2=False
Configure LPSC=False
Configure Pinmux=False
Enable CRC=False
Specify Entrypoint=False
Enable Sequential Read=False
Use 4.5 Clock Divider=False
Use DDR2 Direct Clock=False
Use mDDR=True
ROM ID=1
Device Type=0
Input Clock Speed=24
Clock Type=0
PLL0 Pre Divider=1
PLL0 Multiplier=20
PLL0 Post Divider=2
PLL0 Div1=1
PLL0 Div3=3
PLL0 Div7=6
PLL1 Multiplier=20
PLL1 Post Divider=2
PLL1 Div1=1
PLL1 Div2=2
PLL1 Div3=3
Entrypoint=0
SDRAM SDBCR=0
SDRAM SDTMR=0
SDRAM SDRSRPDEXIT=0
SDRAM SDRCR=0
DDR2 PHY=0
DDR2 SDCR=0
DDR2 SDCR2=0
DDR2 SDTIMR=0
DDR2 SDTIMR2=0
DDR2 SDRCR=0
LPSC0 Enable=
LPSC0 Disable=
LPSC0 SyncRst=
LPSC1 Enable=
LPSC1 Disable=
LPSC1 SyncRst=
Pinmux=
App File String=C:\Project\Metronics\Loader - 45536\Work\BOOTLOADER\aisig\BOOTLOADER.elf
AIS File Name=C:\Project\Metronics\Loader - 45536\Work\BOOTLOADER\aisig\BOOTLOADER.bin