This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error inserting CMEMK->Bad address



Hi, while booting DVSDK-4.01 from SD card onto Beagleboard-xM Rev C, i am facing CMEM error, as mentioned below,

CMEMK module: built on Aug 22 2011 at 18:23:25
  Reference Linux version 2.6.32
  File /home/cedt/DVSDK_Beagle/ti-dvsdk_dm3730-evm_4_01_00_09/linuxutils_2_25_05_11/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0x83700000) overlaps kernel (0x80000000 -> 0xa0000000)
CMEMK Error: Failed to request_mem_region(0x83700000, 35651584)
FATAL: Error inserting cmemk (/lib/modules/2.6.32/kernel/drivers/dsp/cmemk.ko): Bad address
DSPLINK Module (1.65.00.02) created on Date: Aug 22 2011 Time: 18:23:46
SDMAK module: built on Aug 22 2011 at 18:23:26
  Reference Linux version 2.6.32
  File /home/cedt/DVSDK_Beagle/ti-dvsdk_dm3730-evm_4_01_00_09/linuxutils_2_25_05_11/packages/ti/sdo/linuxutils/sdma/src/module/sdmak.c
Starting Matrix GUI application.
I have attached the bootarguments file and my bootlog file too.
https://e2e.ti.com/<a target="_blank">http://e2e.ti.com/cfs-file.ashx/__key/CommunityServer-Discussions-Components-Files/447/2705.bootarguments.txt</a>
https://e2e.ti.com/<a target="_blank">http://e2e.ti.com/cfs-file.ashx/__key/CommunityServer-Discussions-Components-Files/447/0045.bootlog.txt</a>
Please, help me out in solving this CMEM error.

I tired changing the bootarguments value, but nothing is working. So, please suggest what should i do to solve this error.

Thankyou,
Naveen
  • Hi,

    what are the bootargs value you have set? did you also set the mem value?

    Best Regards

    Prabhakar Lad

  • Hello Prabhakar, I have attached the bootargs file and bootlog files

    1781.bootarguments.txt

    0083.bootlog.txt

    There was no any such variable called "mem" in the bootarguments?

    Thank-you,

    Naveen

  • Hi 

     

    looks like you are booting from SD card. does the system directly boots up or does the bootloader comes up and waits for passing arguments?

    Best Regards

    Prabhakar Lad 

  • Hello,

    Yes i do boot from SD card. The system directly boots up. I have pasted the boot arguments of my beagle board XM C

    baudrate=115200
    beaglerev=xMC
    bootcmd=if mmc rescan ${mmcdev}; then if userbutton; then setenv bootenv user.txt;fi;echo SD/MMC found on device ${mmcdev};if run loadbootenv; then echo Loaded environment from ${bootenv};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;if run loaduimage; then run mmcboot;fi;fi;run nandboot;
    bootdelay=3
    bootenv=uEnv.txt
    buddy=none
    camera=lbcm3m1
    console=ttyS2,115200n8
    defaultdisplay=dvi
    dieid#=3ce800029ff800000160a74505018019
    dvimode=640x480MR-16@60
    importbootenv=echo Importing environment from mmc ...; env import -t $loadaddr $filesize
    loadaddr=0x80200000
    loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenv}
    loadramdisk=fatload mmc ${mmcdev} ${rdaddr} ramdisk.gz
    loaduimage=ext2load mmc ${mmcdev}:2 ${loadaddr} /boot/uImage
    loaduimagefat=fatload mmc ${mmcdev} ${loadaddr} uImage
    mmcargs=setenv bootargs console=${console} ${optargs} mpurate=${mpurate} buddy=${buddy} camera=${camera} vram=${vram} omapfb.mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} root=${mmcroot} rootfstype=${mmcrootfstype}
    mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
    mmcdev=0
    mmcroot=/dev/mmcblk0p2 rw
    mmcrootfstype=ext3 rootwait
    mpurate=auto
    nandargs=setenv bootargs console=${console} ${optargs} mpurate=${mpurate} buddy=${buddy} camera=${camera} vram=${vram} omapfb.mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} root=${nandroot} rootfstype=${nandrootfstype}
    nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000 400000; bootm ${loadaddr}
    nandroot=/dev/mtdblock4 rw
    nandrootfstype=jffs2
    ramargs=setenv bootargs console=${console} ${optargs} mpurate=${mpurate} buddy=${buddy} camera=${camera} vram=${vram} omapfb.mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} root=${ramroot} rootfstype=${ramrootfstype}
    ramboot=echo Booting from ramdisk ...; run ramargs; bootm ${loadaddr}
    ramroot=/dev/ram0 rw ramdisk_size=65536 initrd=0x81000000,64M
    ramrootfstype=ext2
    rdaddr=0x81000000
    usbtty=cdc_acm
    vram=12M
  • Can anyone tell me where this insert cmemk.ko start from phys_start (0x83700000)?

    I checked all the loadmodule*.sh file in the file system, and no one has phys_start from 0x83700000.

     

    Regards

    Touse

  • I got the location of the initialized script, it's located in /etc/rc5.d/S99loadmodule-rc

    To avoid the overlap error, just modify the phys_start and phys_end address.

    i.e

    modprobe cmemk phys_start=0x83700000 phys_end=0x85900000