Other Parts Discussed in Thread: OMAP3530
I'm having some trouble getting the burst mode working for an FPGA device. The device is configured as a 16-bit NOR flash device with multiplexed address/data.
I can get it to do a burst of 4 words, which is 64-bits. But it looks like the processor core is breaking my 16 word requests into 4x4 word requests. I think there is some configuration I need to set to get the processor to generate a 16 word burst request to the GPMC module. The GPMC module looks like it is setup correctly. How do I get the core processor to generate the burst request longer than 64-bits?
Below is my current GPMC configuration and code that I am using to generate the read instructions.
/*** ARM assembly to generate 16-word16 burst ***/
asm volatile (
"ldmia %[in]!, {r3-r10} \n\t" // read 16 words from address(ss)
"stmia %[out]!, {r3-r10} \n\t" // write 16 words to address(dest32)
:[out]"+r" (dest32)
:[in]"r" (ss) // address(ss) points to GPMC memory location should do a burst of 16-words from GPMC attached device
:"r3","r4","r5","r6","r7","r8","r9","r10","memory"
);
/***** Config Below ******/
/*
GPMC_CONFIG1: 0x6A001202
31: WRAPBURST = 0 // synchronous wrapping burst not supported
30: READMULTIPLE = 1 // Multiple Access = 1 (Burst if synchronous, page if asynchronous)
29: READTYPE = 1 // Read Synchronous = 1
28: WRITEMULTIPLE = 0 // Single Access
27: WRITETYPE = 1 // Write Asynchronous
26:25: CLKACTIVATIONTIME = 1 // First rising edge of GPMC_CLK at start access time
24:23: ATTACHDDEVICEPAGELENGTH = 2 // 0 is 4 words, 2 is 16 words
22: WAITREADMONITORING = 0 // Wait pin is not monitored for read accesses
21: WAITEWRITEMONITORING = 0 // Wait pin is not monitoried for write accesses
20: Reserved = 0
19:18: WAITMONITORINGTIME = 0 // Wait pin is monitored with valid data
17:16: WAITPINSELECT = 0 // Wait pin is WAIT0
15:14: Reserved = 0
13:12: DEVICESIZE = 1 // 16 bit interface
11:10: DEVICETYPE = 0 // NOR Flash like device
9: MUXADDDATA = 1 // Address and data multiplexed attached device
8:7:6:5 Reserved = 0
4: TIMEPARAGRANULARITY = 0 // x1 latencies
3:2: Reserved
1:0: GPMCFCLKDIVIDER = 2 // GPMC_CLK freq = GPMC_FCLK/2 for 1. GPMC_FCLK/3 for 2
*/
static unsigned int config1 = 0x6B001202;
/*
GPMC_CONFIG2:0x001E1803
31:21: RESERVED = 0
20:16: CSWROFFTIME = 0x1E // 20 GPMC_FCLK cycle CS I de-assertion time from start cycle time for write
15:13: RESERVED = 0
12:8: CSRDOFFTIME = 0x18 // 20 GPMC_FLCK CS I de-assertion time from start cycle time for read
7: CSEXTRADELAY = 0 // CS I Time control signal is not delayed
6:4: RESERVED = 0
3:0: CSONTIME = 3 // 2 GPMC_FCLK cycle CS I assertion time from start cycle
*/
static unsigned int config2 = 0x001E1803;
/*
GPMC_CONTROL3: 0x00080803
31:21: RESERVED = 0
20:16: ADVWROFFIME = 8 // 4 GPMC_FCLK cycle nADV de-assertion time from start cycle time for write
15:13: RESERVED = 0
12:8: ADVRDOFFTIME = 8 // 4 GPMC_FCLK cycle nADV de-assertion time from start cycle for read
7: ADVEXTRADELAY = 0 // 0 NO - nADV Add Extra Half GPMC_FLCK
6:4: RESERVED = 0
3:0: ADVONTIME = 3 // 2 GPMC_FCLK cycle nADV assertion time from start cycle
*/
static unsigned int config3 = 0x00080803;
/*
GPMC_CONTROL4: 0x1B091509
31:29: RESERVED = 0
28:24: WEOFFTIME = 0x1B // nWE de-assertion time from start cycle (units = GPMC_FCLK)
23: WEEXTRADELAY = 0 // nWE Add Extra Half GPMC_FCLK cycle
22:20: RESERVED = 0
19:16: WEONTIME = 9 // nWE assertin time from start cycle time (units = GPMC_FCLK)
15:13: RESERVED = 0
12:8: OEOFFTIME = 0x15 // nOE de-assertion time from start cycle time (units = GPMC_FCLK)
7: OEEXTRADELAY = 0 // nOE Add Extra Half GPMC_FCLK cycle
6:4: RESERVED = 0
3:0: OEONTIME = 9 // nOE assertion time from start cycle time
*/
static unsigned int config4 = 0x1B091509;
/*
GPMC_CONTROL5: 0x05151e18
31:28: RESERVED = 0
27:24: PAGEBURSTACCESSTIME = 3 // Delay between successive words in a multiple address
23:21: RESERVED = 0
20:16: RDACCESSTIME = 0x15 // Delay between start cycle time and first data valid (GPMC_FCLK cycles)
15:13: RESERVED = 0
12:8: WRCYCLETIME = 0x1E // Total write cycle time (GPMC_FCLK cycles)
7:5: RESERVED = 0
4:0: RDCYCLETIME = 0x18 // Total read cycle time (GPMC_FCLK cycles)
*/
static unsigned int config5 = 0x03151e18;
/*
GPMC_CONTROL6:0x92090000
31: RESERVED = 1
30:29: RESERVED = 0
28:24: WRACCESSTME = 0x12 // Delay from start access time to the GPMC_FCLK rising edge
23:20: RESERVED = 0
19:16: WRDATAONADMUXBUS = 9 // Specifies on which GPMC_FCLK rising edge the first data
// the synchronous burst write is driven in the add/data mux bus
15:12: RESERVED = 0
11:8: CYCLE2CYCLEDELAY = 0 // Chip-select high pulse delay between successive accesses (GPMC_FCLK)
7: CYCLE2CYCLESAMECSEN = 0 // Add CYCLE2CYCLEDELAY between successive accesses to the same CS
6: CYCLE2CYCLEDIFFCSEN = 0 // Add CYCLE2CYCLEDELAY between successive accesses to a different CS
5:4: RESERVED = 0
3:0 BUSTURNAROUND = 0 // Bus turn arround latency (GPMC_FCLK cycles)
*/
static unsigned int config6 = 0x92090000;
/*
GPMC_CONTROL7: 0x00000F68
31:12 RESERVED = 0
11:8: MASKADDRESS = 0xF // CS mask address chip-select size of 16 Mbytes
7: RESERVED = 0
6: CSVALID = 1 // CS enable must be disabled when writing to BASEADDRESS
5:0: BASEADDRESS = 0x28 // CS base address bits[2:0] correspond to A26, A25 and A24
// CS4 on OMAP3EVM address is 0x28000000
*/
/* enable cs */
static unsigned int config7 = 0x00000F68;