I want to know that the CMOS camera can be interfaced with the LCDK 6748 and OMAP L138 or not,,,,if not then which type of camera can be interfaced with these kits
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to know that the CMOS camera can be interfaced with the LCDK 6748 and OMAP L138 or not,,,,if not then which type of camera can be interfaced with these kits
Hi,
Available Camera Interfaces on C6748/OMAPL138 LCDK:
Refer the below wiki to get the more info.
http://processors.wiki.ti.com/index.php/LCDK_User_Guide
http://processors.wiki.ti.com/index.php/L138/C6748_Development_Kit_(LCDK)
http://processors.wiki.ti.com/index.php/BIOS_C6SDK_2.0_Getting_Started_Guide