The example program listed below takes input from line in and send back the same to line out. What I am willing is to take input from MIC and do the rest same. What change should I make. I am newbie to the dsp6713 & not following Rulph chassing for some reason.
/*
* Copyright 2003 by Texas Instruments Incorporated.
* All rights reserved. Property of Texas Instruments Incorporated.
* Restricted rights to use, duplicate or disclose this code are
* granted through contract.
*
*/
/* "@(#) DSP/BIOS 4.90.270 01-08-04 (bios,dsk6713-c04)" */
/*
* ======== tsk_audio.c ========
*
* This example demonstrates the use of IOM drivers with SIOs and tasks by
* using the DIO class driver with a user defined device mini-driver
* called "codec" and a class driver DIO instance called "dio_codec". This is
* the loopback application where audio is read from an input SIO, then sent
* back via an output SIO.
* The following objects need to be created in the DSP/BIOS
* configuration for this application:
*
* * A UDEV object, which links in a user device driver. In this
* case the UDEV is a codec based IOM device driver.
* * A DIO object, which links the UDEV object.
* * A TSK object, with the function to run set to the function echo
* defined in this file.
* * A LOG named trace for debug and status output.
*/
#include <std.h>
#include <math.h>
#include <log.h>
#include <sys.h>
#include <mem.h>
#include <sio.h>
#ifdef _6x_
extern far LOG_Obj trace;
extern anc_asm_func();
/*
* Buffers placed in external memory are aligned on a 128 bytes boundary.
* In addition, the buffer should be of a size multiple of 128 bytes for
* the cache work optimally on the C6x.
*/
#define BUFLEN 128 /* number of samples in the frame */
#define BUFALIGN 128 /* alignment of buffer to allow use of L2 cache */
#else
extern LOG_Obj trace;
#define BUFLEN 128 /* number of samples in the frame */
#define BUFALIGN 1
#endif
#define BUFSIZE (BUFLEN * sizeof(MdUns))
/* inStream and outStream are SIO handles created in main */
SIO_Handle inStream, outStream;
/* Function prototype */
static Void createStreams();
static Void prime();
/*
* ======== main ========
*/
Void main()
{
int i;
LOG_printf(&trace, "tsk_audio started");
}
/*
* ======== createStreams ========
*/
static Void createStreams()
{
SIO_Attrs attrs;
/* align the buffer to allow it to be used with L2 cache */
attrs = SIO_ATTRS;
attrs.align = BUFALIGN;
attrs.model = SIO_ISSUERECLAIM;
/* open the I/O streams */
inStream = SIO_create("/dioCodec", SIO_INPUT, BUFSIZE, &attrs);
if (inStream == NULL) {
SYS_abort("Create input stream FAILED.");
}
outStream = SIO_create("/dioCodec", SIO_OUTPUT, BUFSIZE, &attrs);
if (outStream == NULL) {
SYS_abort("Create output stream FAILED.");
}
}
/*
* ======== prime ========
*/
static Void prime()
{
Ptr buf0, buf1, buf2, buf3;
LOG_printf(&trace, "Allocate buffers started");
/* Allocate buffers for the SIO buffer exchanges */
buf0 = (Ptr)MEM_calloc(0, BUFSIZE, BUFALIGN);
buf1 = (Ptr)MEM_calloc(0, BUFSIZE, BUFALIGN);
buf2 = (Ptr)MEM_calloc(0, BUFSIZE, BUFALIGN);
buf3 = (Ptr)MEM_calloc(0, BUFSIZE, BUFALIGN);
if (buf0 == NULL || buf1 == NULL || buf2 == NULL || buf3 == NULL) {
SYS_abort("MEM_calloc failed.");
}
/* Issue the first & second empty buffers to the input stream */
if (SIO_issue(inStream, buf0, SIO_bufsize(inStream), NULL) != SYS_OK) {
SYS_abort("Error issuing buffer to the input stream");
}
if (SIO_issue(inStream, buf1, SIO_bufsize(inStream), NULL) != SYS_OK) {
SYS_abort("Error issuing buffer to the input stream");
}
/* Issue the first & second empty buffers to the output stream */
if (SIO_issue(outStream, buf2, SIO_bufsize(outStream), NULL) != SYS_OK) {
SYS_abort("Error issuing buffer to the output stream");
}
if (SIO_issue(outStream, buf3, SIO_bufsize(outStream), NULL) != SYS_OK) {
SYS_abort("Error issuing buffer to the output stream");
}
}
/*
* ======== echo ========
* This function copies from the input SIO to the output SIO. You could
* easily replace the copy function with a signal processing algorithm.
*/
Void echo()
{
Int i;
Int nmadus; /* number of minimal addressable units */
MdUns *inbuf, *outbuf;
/* Call createStream function to create I/O streams */
createStreams();
/* Call prime function to do priming */
prime();
/* Loop forever looping back buffers */
for (;;) {
/* Reclaim full buffer from the input stream */
if ((nmadus = SIO_reclaim(inStream, (Ptr *)&inbuf, NULL)) < 0) {
SYS_abort("Error reclaiming full buffer from the input stream");
}
/* Reclaim empty buffer from the output stream to be reused */
if (SIO_reclaim(outStream, (Ptr *)&outbuf, NULL) < 0) {
SYS_abort("Error reclaiming empty buffer from the output stream");
}
/* Do the data move. */
for (i = 0; i < (nmadus / sizeof(short)); i++) {
outbuf[i] = inbuf[i];
}
/* Issue full buffer to the output stream */
if (SIO_issue(outStream, outbuf, nmadus, NULL) != SYS_OK) {
SYS_abort("Error issuing full buffer to the output stream");
}
/* Issue an empty buffer to the input stream */
if (SIO_issue(inStream, inbuf, SIO_bufsize(inStream), NULL) != SYS_OK) {
SYS_abort("Error issuing empty buffer to the input stream");
}
}
}
/*
* ======== prd10secs ========
* prd10secs is configured to be called every 10 seconds
*/
Void prd10secs()
{
static Int seconds = 0;
static Int minutes = 0;
static Int hours = 0;
seconds += 10;
if (seconds == 60) {
seconds = 0;
minutes++;
if (minutes == 60) {
minutes = 0;
hours++;
}
LOG_printf(&trace, "%d hours and %d minutes", hours, minutes);
}
else {
LOG_printf(&trace, "%d seconds", seconds);
}
}