I have this sample code to generate a sine wave of 1 KHZ which i received from TI.
I would like to know how to do the hexadecimal calculation to produce a wave of 610HZ.
#include "tonecfg.h"
#include "dsk6713.h"
#include "dsk6713_aic23.h"
/* Length of sine wave table */
#define SINE_TABLE_SIZE 48
/* Codec configuration settings */
DSK6713_AIC23_Config config = { \
0x0017, /* 0 DSK6713_AIC23_LEFTINVOL Left line input channel volume */ \
0x0017, /* 1 DSK6713_AIC23_RIGHTINVOL Right line input channel volume */\
0x00d8, /* 2 DSK6713_AIC23_LEFTHPVOL Left channel headphone volume */ \
0x00d8, /* 3 DSK6713_AIC23_RIGHTHPVOL Right channel headphone volume */ \
0x0011, /* 4 DSK6713_AIC23_ANAPATH Analog audio path control */ \
0x0000, /* 5 DSK6713_AIC23_DIGPATH Digital audio path control */ \
0x0000, /* 6 DSK6713_AIC23_POWERDOWN Power down control */ \
0x0043, /* 7 DSK6713_AIC23_DIGIF Digital audio interface format */ \
0x0081, /* 8 DSK6713_AIC23_SAMPLERATE Sample rate control */ \
0x0001 /* 9 DSK6713_AIC23_DIGACT Digital interface activation */ \
};
/* Pre-generated sine wave data, 16-bit signed samples */
Int16 sinetable[SINE_TABLE_SIZE] = {
0x0000, 0x10b4, 0x2120, 0x30fb, 0x3fff, 0x4dea, 0x5a81, 0x658b,
0x6ed8, 0x763f, 0x7ba1, 0x7ee5, 0x7ffd, 0x7ee5, 0x7ba1, 0x76ef,
0x6ed8, 0x658b, 0x5a81, 0x4dea, 0x3fff, 0x30fb, 0x2120, 0x10b4,
0x0000, 0xef4c, 0xdee0, 0xcf06, 0xc002, 0xb216, 0xa57f, 0x9a75,
0x9128, 0x89c1, 0x845f, 0x811b, 0x8002, 0x811b, 0x845f, 0x89c1,
0x9128, 0x9a76, 0xa57f, 0xb216, 0xc002, 0xcf06, 0xdee0, 0xef4c
};
/*
* main() - Main code routine, initializes BSL and generates tone
*/
void main()
{
DSK6713_AIC23_CodecHandle hCodec;
Int16 msec, sample;
/* Initialize the board support library, must be called first */
DSK6713_init();
/* Start the codec */
hCodec = DSK6713_AIC23_openCodec(0, &config);
/* Generate a 1KHz sine wave for 5 seconds */
for (msec = 0; msec < 5000; msec++)
{
for (sample = 0; sample < SINE_TABLE_SIZE; sample++)
{
/* Send a sample to the left channel */
while (!DSK6713_AIC23_write(hCodec, sinetable[sample]));
/* Send a sample to the right channel */
while (!DSK6713_AIC23_write(hCodec, sinetable[sample]));
}
}
/* Close the codec */
DSK6713_AIC23_closeCodec(hCodec);
}