Other Parts Discussed in Thread: OMAPL138
Hi there,
I want to use an SPI interface on the C6748 LCDK evaluation board. Unfortunately there is no info about it in SPRT633, and also not on the wiki page http://processors.wiki.ti.com/index.php/L138/C6748_Development_Kit_(LCDK).
The C6748 DSP has two Serial Peripheral Interface Ports (SPI0, SPI1).
Only the finger print sensor is mentioned, which afair was connected through SPI. The block diagram states a connection through SPI1. SPI0 is not listed there.
Even though there are schematics in sprcaf4_LCDK.zip (VER A7E) I could not figure out if SPI0 or SPI1 can be used on this board. Some signals seem to be connected to connector J16. A also could not find connector J16 on the board, and unfortunately the Assy_bot.pdf and Assy_top.pdf cannot be searched for those names.
Finally with help of the BOM entry "CONN FPC/FFC 36POS .5MM VERT ZIF, Molex" I could find it. It is the camera cable connector next to the yellow composite socket which indeed is labeled "J16". Is this correct?
Any guidance is very much appreciated. Thanks!
Best regards,
Matthias