This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713: suggestion for input and output port

Part Number: TMS320C6713


Working on TMS320C6713 kit have to connect Rscad digital output to kit and from which pin of expansion connector  i can take output 

please tell me which "digital input and output to expansion connector" i can  refer to? Please see the expansion connector of DSK6713 on below website.
http://c6000.spectrumdigital.com/dsk6713/revc/files/6713_dsk_techref.pdf . 

and which expansion connector to use J1 , J3 , J4  . which one is used for what purpose .

  • Hi Aman,

    I've forwarded this to the design team. Their feedback should be posted here.

    BR
    Tsvetolin Shulev
  • Aman,

    The HPI interface data pins are multiplexed with GPIO, these pins are connected to J1 connector. Please refer C6713 DSK schematics page 6 to know about the connections.

    Regards,
    Senthil
  • Aman,

    Your description and questions are very vague. For us to help you, you will need to describe some analysis of your system to detail the type of digital signals you need from your "Rscad digital output" and then you will need to detail the type of digital outputs you need from the DSK6713. Since you know what you are trying to do with the kit, you can do this and we cannot.

    The datasheet lists all the types of digital input and output that the C6713 can support, and the Tech Ref shows which ones go to the Expansion header. You will be able to select from those to get the signals that can be used in the system.

    Regards,
    RandyP