I'm using the DSPLIB_C67x to do the FFT Algo. I counldn't find the windowing function.
Does this LIB have the windowing function?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We don`t provide Windowing function in DSPLIB as the loops are simple enough to implement in C and the compiler does a good job provided you provide the correct _nassert and PRAGMA statements to guide the compiler.
For example the 2k sample hanning window implementation would be :
vecSize =2048;
_nassert(vecSize % 8 == 0 ); // window size is always multiple of 8
_nassert(vecSize > 0); // window size is always greater than 0
_nassert((int)DataOut % 8 == 0); // data is double word aligned
_nassert((int)DataInput % 8 == 0); // data is double word aligend
#pragma MUST_ITERATE(64,8192,64);
for ( i = 0; i < vecSize; i++) {
double mult= 0.5 * (1 - cos(2*PI*i/2047));
DataOut[i] = mult * DataInput[i];
}
BAsed on the implementation described here:
en.wikipedia.org/.../Hann_function
Add restricts to input and output data and the compiler should generate optimized data.
Regards,
Rahul
PS: Look at path for least resistance to optimize DSP code:
www.ti.com/.../sprabf2.pdf
Marcelo,
Please don`t post unrelated part number selection question on an old e2e thread related to DSPLIB.
We have replied to your query regarding performance audio part selection here:
e2e.ti.com/.../2185794
Regards,
Rahul