Other Parts Discussed in Thread: SPRC203
Hello:
I used a PADK EVM.When I wanted to try the bootloader from prallel flash,I had a trouble in process.I followed the operation in PDF of PADK. In D:\Lyrtech\PADK\bootload\flash\makerom,there are a makerom.exe.The pdf requires proceed as
follows.
1. Copy the .out file of a working application to the Makerom folder.
2. Run MakeRom.exe Updater.out <application_name> in a command shell.
This creates a file named FLASH_<application_name>.out.
3. Use Code Composer Studio to upload and run this file on the PADK.
4. Make sure that the PADK is set to boot from the flash memory.
5. Reset the PADK to run the programmed application.
So I made a FLASH_SwitchesAndLeds.out with the provided example that named SwitchesAndLeds.
But after these operations,when I run the FLASH_SwitchesAndLeds.out,the CCS4 told me "the main() in the Updater.c were Unfound".And the PADK doesn't provide the soucecodes.So the bootloader didn't success.
Could you give me some help?Thanks very much!