This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot load sources to my UBUNTU system

Based on TI's documentation for Android on the AM37X I followed the doc till the following:

Using pre-packaged repo

The above method is ideal but is time consuming, so developers can use the pre-packaged Android sources in DevKit package.

NOTE: Once the sources are generated developers can do a “repo sync” to pull latest updates (if any) from gitorious.org/rowboat

  $ mkdir rowboat-android
  $ cd rowboat-android
  $ Download the pre-packaged repo from http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_4_DevKit_2_1/index_FDS.html
  $ tar -xvzf 	TI_Android_GingerBread_2_3_4Sources.tar.gz
  $ cd 	TI_Android_GingerBread_2_3_4Sources
  $ ./.repo/repo/repo sync --local-only

The last command fails as follows:
s$ ./.repo/repo/repo sync --local-only
Traceback (most recent call last):
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/main.py", line 238, in <module>
    _Main(sys.argv[1:])
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/main.py", line 220, in _Main
    repo._Run(argv)
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/main.py", line 118, in _Run
    use_pager = config.GetBoolean('pager.%s' % name)
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/git_config.py", line 98, in GetBoolean
    v = self.GetString(name)
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/git_config.py", line 115, in GetString
    v = self._cache[_key(name)]
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/git_config.py", line 223, in _cache
    self._cache_dict = self._Read()
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/git_config.py", line 229, in _Read
    d = self._ReadGit()
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/git_config.py", line 280, in _ReadGit
    d = self._do('--null', '--list')
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/git_config.py", line 304, in _do
    capture_stderr = True)
  File "/home/narayan/rowboat-android/TI_Android_GingerBread_2_3_4Sources/.repo/repo/git_command.py", line 212, in __init__
    raise GitError('%s: %s' % (command[1], e))
error.GitError: config: [Errno 2] No such file or directory
Does anybody have an idea why? I am following the TI documentation under
I am running UBUNTU as a VM under VMWare. The UBUNTU version is 11
Thanks in Advance.
Narayan