This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VNC screen cuts from right Side after changed in resolution.

Hi All,

As per this question i changed in kernel source code and able to changed vnc solution as per requirement. But still here i am facing one problem about this. in vnc it cuts right side part. you can see result in image also.

http://e2e.ti.com/support/embedded/android/f/509/p/291228/1016681.aspx#1016681

Vnc part is cuts from right hand side.

Any can please tell me whats wrong here.

Output of console :

Initializing grabber method...
No grabber method selected, auto-detecting...
--Loading flinger native lib--
Loading lib: /data/data/org.onaips.vnc/lib//libdvnc_flinger_sdk15.so
Couldnt load flinger library /data/data/org.onaips.vnc/lib//libdvnc_flinger_sdk15.so! Error string: (null)
Loading lib: /data/data/org.onaips.vnc/lib//libdvnc_flinger_sdk17.so
AKI1
--Initializing gingerbread access method--
AKII12AKI2
Initializing vir[ 3291.433319] input: QuipmentTouchscreen as /devices/virtual/input/input1
tual keyboard and touch device...
---Initializing uinput...---
Initializing VNC server:
        width:  800
        height: 480
        bpp:    32
        port:   5901
Colourmap_rgba=0:8:16:24    lenght=8:8:8:8
Version: DEVILISH DONKEY
23/09/2013 11:10:38 Listening for VNC connections on TCP port 5901
Starting IPC connection...binded to port 13132

Waiting for a connection

Thanks