Other Parts Discussed in Thread: DM385
Hi there,
After having issues with JFFS2 and Hamming HW ECC on the DM8148 and our NAND, I switched to BCH8 + UBIFS, per the solution in this thread.
I got the BCH8 + UBIFS running, but I'm still seeing ECC errors, such as the following.
UBI error: ubi_io_read: error -74 (ECC error) while reading 129024 bytes from PEB 449:2048, read 129024 bytes
UBI error: ubi_io_read: error -74 (ECC error) while reading 131072 bytes from PEB 1813:0, read 131072 bytes
UBI error: torture_peb: read problems on freshly erased PEB 1813, must be bad
UBI error: erase_worker: failed to erase PEB 1813, error -5
UBI: mark PEB 1813 as bad
UBI: 17 PEBs left in the reserve
After a number of reboots, all PEBs reserved for bad blocks are used, and the filesytems goes into a read-only mode. (We'll need it to be RW in our application.)
The procedure I followed was:
-
Start with EZSDK 5.05.02.00
-
Fetch master from linux-omap3.git so I have all the lastest NAND/ECC related patches. (At the time of this post, [master] and [ti81xx-master] are @ 5efb81ac9e9b0c72a8e4edf159b7b5e06980ee56. I added my defconfig and updated the EZSDK make rules to point to this kernel, and did a clean build.
-
Take my existing rootfs and create my ubi image. Here are my notes on this, which shows the parameter used. It appears that our device supports 512-byte subppages. 3808.ubifs_notes.txt
[Update - The PEB --> LEB conversion in my attached notes is wrong: It should be 128 KiB / 126 KiB] -
Flash the ubi image and boot the system as shown in the attached log.In this log you'll see the ECC errors and PEBs being marked bad at each reboot. 7838.ecc_error_log.txt
[Update - Please see the log from the next post instead; it is more up-to-date]
In the meantime, I'm going to try switching to SW ECC to rule out any HW ECC issues. I'll post back with those results as soon as I can.
Has anyone else resolved this issue? I've seen a number of similar threads without clear solutions. However, I'm not sure if they ended up using the latest in linux-omap3.git. If anyone could provide some advice on isolating and addressing this issue, it would be greatly appreciated.
Thank you!
Jon