Hi Using EVM6678 I have followed the instruction in http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#Example_2_-_Building_and_running_your_first_tasking_application_using_MCSDK_and_BIOS and build a simple project to blink led and using jtag it tun properly on core 1, but when i configure swithes to boot from NAND and use mcoreloader to load led_playbios.out file to core1 there is the following error: / # mcoreloader 1 /var/local/led_playbios.out ELF: ELF ELF file header entry point: c013dc0 << D L O A D >> ERROR: Failed to set target memory for segment. << D L O A D >> ERROR: Failed to allocate target memory for static executable. Failed to load file /var/local/led_playbios.out on core 1 what is the problem with my work? I use led_playbios.out directly from the output of build procedure in CCS, is it correct? is it any conversion needed to convert this .out file to .xe66> thanks