This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question on exFAT filesystem support



Hi my customer want to using exFAT FS on nand/SD.   The platform is DM8127 + IPNCRDK3.5

Is it possible to support exFAT FS on current kernel?

BR,

Eason

  • Hi Eason,

    I think, you can use extFS support in SD/USB etc., not through NAND flash.

    You have to cross compile the "fuse-exfat" (mount support) and "extfs-utils" packages to support "extFS".

    Try the below link to enable extFS support in kernel.

    https://github.com/dorimanx/exfat-nofuse

  • Hi Thanks for reply!

    Could you let me know why exFAT on NAND is not supported?

    BR,

    Eason

  • Hi Eason,

    EXT filesystem doesn't support journaling fs and "power loss safe".

    JFFS2,YAFFS2,UBIFS are the filesystems used in flash memory devices such as NAND, NOR, etc.,

    EXT fs is used in eMMC/SD/MMC/HDD etc., which is doesn't care about power loss. ex: Desktop based

    Refer to the below link.

    http://www.micron.com/~/media/Documents/Products/Software%20Article/SWNL_choosing_linux_fs_for_flash.pdf

    Chapter "Sector-Based Read/Write File Systems" and "Power Loss Tolerance"

  • Appreciate for your help!

    Regards,

    Eason

  • Hi Eason,

    I'm able to enable "extFS" support in liunux kernel and able to mount (pendrive) too.

    Steps:

    1) Download the "exFAT" moudule linux driver from the below link.

    https://github.com/dorimanx/exfat-nofuse

    2) Modify the "Makefile" as per your kernel source.

    3) Build with your tollchain

    4) Install the "exFAT" driver in linux.

    Build Log:

    titus@Titus:~/workdir/ti-e2e/exfat-nofuse-master$ make ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi-
    make -C /opt/ti/mcsdk_1_01_00_01/board-support/linux-3.3-psp03.22.00.06.sdk M=/home/titus/workdir/ti-e2e/exfat-nofuse-master modules
    make[1]: Entering directory `/opt/ti/mcsdk_1_01_00_01/board-support/linux-3.3-psp03.22.00.06.sdk'
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_core.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_super.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_api.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_blkdev.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_cache.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_data.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_bitmap.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_nls.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_oal.o
      CC [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat_upcase.o
      LD [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat.o
      Building modules, stage 2.
      MODPOST 1 modules
      CC      /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat.mod.o
      LD [M]  /home/titus/workdir/ti-e2e/exfat-nofuse-master/exfat.ko
    make[1]: Leaving directory `/opt/ti/mcsdk_1_01_00_01/board-support/linux-3.3-psp03.22.00.06.sdk'
    titus@Titus:~/workdir/ti-e2e/exfat-nofuse-master$

    Makefile:

    #
    # Makefile for Linux FAT12/FAT16/FAT32(VFAT)/FAT64(ExFAT) filesystem driver.
    #
    
    ifneq ($(KERNELRELEASE),)
    # call from kernel build system
    
    obj-$(CONFIG_EXFAT_FS) += exfat.o
    
    exfat-objs := exfat_core.o exfat_super.o exfat_api.o exfat_blkdev.o exfat_cache.o \
    			   exfat_data.o exfat_bitmap.o exfat_nls.o exfat_oal.o exfat_upcase.o
    
    else
    # external module build
    
    EXTRA_FLAGS += -I$(PWD)
    
    #
    # KDIR is a path to a directory containing kernel source.
    # It can be specified on the command line passed to make to enable the module to
    # be built and installed for a kernel other than the one currently running.
    # By default it is the path to the symbolic link created when
    # the current kernel's modules were installed, but
    # any valid path to the directory in which the target kernel's source is located
    # can be provided on the command line.
    #
    #KDIR	:= /lib/modules/$(shell uname -r)/build
    KDIR	:= /opt/ti/mcsdk_1_01_00_01/board-support/linux-3.3-psp03.22.00.06.sdk
    MDIR	:= /usr/local/filesystem_omapl138/lib/modules/$(shell uname -r)
    PWD	:= $(shell pwd)
    KREL	:= $(shell cd ${KDIR} && make -s kernelrelease)
    MDIR	:= /usr/local/filesystem_omapl138/lib/modules/${KREL}
    PWD	:= $(shell pwd)
    
    export CONFIG_EXFAT_FS := m
    
    all:
    	$(MAKE) -C $(KDIR) M=$(PWD) modules
    
    clean:
    	$(MAKE) -C $(KDIR) M=$(PWD) clean
    
    help:
    	$(MAKE) -C $(KDIR) M=$(PWD) help
    
    install: exfat.ko
    	rm -f ${MDIR}/kernel/fs/exfat/exfat.ko
    	install -m644 -b -D exfat.ko ${MDIR}/kernel/fs/exfat/exfat.ko
    	depmod -aq
    
    uninstall:
    	rm -rf ${MDIR}/kernel/fs/exfat
    	depmod -aq
    
    endif
    
    .PHONY : all clean install uninstall

     

    Log:


    root@omapl138-lcdk:/# cat /proc/filesystems
    nodev   sysfs
    nodev   rootfs
    nodev   bdev
    nodev   proc
    nodev   cgroup
    nodev   tmpfs
    nodev   debugfs
    nodev   sockfs
    nodev   pipefs
    nodev   anon_inodefs
    nodev   rpc_pipefs
    nodev   devpts
            ext3
            ext2
            cramfs
    nodev   ramfs
            vfat
            msdos
            iso9660
    nodev   nfs
            ufs
    nodev   jffs2
    nodev   mqueue
    nodev   mtd_inodefs
    nodev   ubifs
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/# insmod exfat.ko
    exFAT: Version 1.2.9
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/# cat /proc/filesystems
    nodev   sysfs
    nodev   rootfs
    nodev   bdev
    nodev   proc
    nodev   cgroup
    nodev   tmpfs
    nodev   debugfs
    nodev   sockfs
    nodev   pipefs
    nodev   anon_inodefs
    nodev   rpc_pipefs
    nodev   devpts
            ext3
            ext2
            cramfs
    nodev   ramfs
            vfat
            msdos
            iso9660
    nodev   nfs
            ufs
    nodev   jffs2
    nodev   mqueue
    nodev   mtd_inodefs
    nodev   ubifs
            exfat
    root@omapl138-lcdk:/# usb 1-1: new full-speed USB device number 2 using ohci
    usb 1-1: not running at top speed; connect to a high speed hub
    scsi1 : usb-storage 1-1:1.0
    scsi 1:0:0:0: Direct-Access     Generic  Mass Storage     1.00 PQ: 0 ANSI: 2
    sd 1:0:0:0: Attached scsi generic sg0 type 0
    sd 1:0:0:0: [sda] 16179200 512-byte logical blocks: (8.28 GB/7.71 GiB)
    sd 1:0:0:0: [sda] Write Protect is off
    sd 1:0:0:0: [sda] Asking for cache data failed
    sd 1:0:0:0: [sda] Assuming drive cache: write through
    sd 1:0:0:0: [sda] Asking for cache data failed
    sd 1:0:0:0: [sda] Assuming drive cache: write through
     sda: sda1
    sd 1:0:0:0: [sda] Asking for cache data failed
    sd 1:0:0:0: [sda] Assuming drive cache: write through
    sd 1:0:0:0: [sda] Attached SCSI removable disk

    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/# mountFAT-fs (sda): bogus number of reserved sectors
    FAT-fs (sda): Can't find a valid FAT filesystem
    [EXFAT] trying to mount...
     [EXFAT] FsMountVol failed

    rootfs on / type rootfs (rw)
    /dev/root on / type ext3 (rw,relatime,errors=continue,user_xattr,barrier=1,data=writeback)
    proc on /proc type proc (rw,relatime)
    tmpfs on /mnt/.splash type tmpfs (rw,relatime,size=40k)
    sysfs on /sys type sysfs (rw,relatime)
    none on /dev type tmpfs (rw,relatime,size=1024k,nr_inodes=8192,mode=755)
    /dev/mmcblk0p2 on /media/mmcblk0p2 type ext3 (rw,relatime,errors=continue,user_xattr,barrier=1,data=writeback)
    /dev/mmcblk0p1 on /media/mmcblk0p1 type vfat (rw,relatime,fmask=0022,dmask=0022,codepage=cp437,iocharset=iso8859-1,shortname=mixed,e)
    /dev/mmcblk0p3 on /media/mmcblk0p3 type ext3 (rw,relatime,errors=continue,user_xattr,barrier=1,data=writeback)
    devpts on /dev/pts type devpts (rw,relatime,gid=5,mode=620)
    tmpfs on /var/volatile type tmpfs (rw,relatime,size=16384k)
    tmpfs on /dev/shm type tmpfs (rw,relatime,mode=777)
    tmpfs on /media/ram type tmpfs (rw,relatime,size=16384k)
    root@omapl138-lcdk:/# FAT-fs (sda1): bogus number of reserved sectors
    FAT-fs (sda1): Can't find a valid FAT filesystem
    [EXFAT] trying to mount...
    [EXFAT] mounted successfully
    nls_utf8: disagrees about version of symbol module_layout

    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/# mount
    rootfs on / type rootfs (rw)
    /dev/root on / type ext3 (rw,relatime,errors=continue,user_xattr,barrier=1,data=writeback)
    proc on /proc type proc (rw,relatime)
    tmpfs on /mnt/.splash type tmpfs (rw,relatime,size=40k)
    sysfs on /sys type sysfs (rw,relatime)
    none on /dev type tmpfs (rw,relatime,size=1024k,nr_inodes=8192,mode=755)
    /dev/mmcblk0p2 on /media/mmcblk0p2 type ext3 (rw,relatime,errors=continue,user_xattr,barrier=1,data=writeback)
    /dev/mmcblk0p1 on /media/mmcblk0p1 type vfat (rw,relatime,fmask=0022,dmask=0022,codepage=cp437,iocharset=iso8859-1,shortname=mixed,e)
    /dev/mmcblk0p3 on /media/mmcblk0p3 type ext3 (rw,relatime,errors=continue,user_xattr,barrier=1,data=writeback)
    devpts on /dev/pts type devpts (rw,relatime,gid=5,mode=620)
    tmpfs on /var/volatile type tmpfs (rw,relatime,size=16384k)
    tmpfs on /dev/shm type tmpfs (rw,relatime,mode=777)
    tmpfs on /media/ram type tmpfs (rw,relatime,size=16384k)
    /dev/sda1 on /media/sda1 type exfat (rw,relatime,fmask=0022,dmask=0022,namecase=1,errors=remount-ro)
    root@omapl138-lcdk:/# ls /media/sda1/
    exfat_test.txt
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/# uname -a
    Linux omapl138-lcdk 3.3.0 #13 PREEMPT Thu Aug 28 17:49:04 IST 2014 armv5tejl unknown
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/#
    root@omapl138-lcdk:/#

  • Hi Many many thanks!

    Because the kernel in IPNCRDK is 2.6.37, the kerenl you mentioned is 3.x, I have suggested my ctm to find kind of patch over linux 2.6.37, and they will try on that first.

    BR,

    Eason