Other Parts Discussed in Thread: AM3352
HI ,
We are using AM3352 processor -- SDK-08 and linux kernel version is 3.14.
we are using pwm-capture driver to read the fanspeed in rpm and that data we want to send to user space application.
#1: This feature is not available/included in SDK-08 -- but i modified the drivers/pwm/sysfs.c and core.c and added few functions --
-- here fanspeed value rpm which is 4 bytes data i need to sent to userspace application.
we tried with copy_to_user -- but it is throwing error --
#include <string.h>
#include <stdio.h>
#include <stdlib.h>
#include <unistd.h>
#include <fcntl.h>
char array[10];
void main()
{
int fd = 0;
char status=0;
fd= open("/sys/class/pwm/pwmchip0/pwm0/ecap_get_rpm", O_RDWR);
printf("fd:%d \n",fd);
status = read(fd, array, 4);
printf("status :%d \n",status);
}
error log:
root@am335x-evm:/usr# ./test-pwm
fd:3
[ 57.115106] pwm_ecap_get_rpm_show:
[ 57.118900] ecap_pwm_get_value:
[ 57.123449] rpm:3000
[ 57.125766] ret:4
[ 57.127796] get:value:0 0 0 0
[ 57.131675] Unable to handle kernel NULL pointer dereference at virtual address 00000000
[ 57.140184] pgd = cc480000
[ 57.143103] [00000000] *pgd=8f687831, *pte=00000000, *ppte=00000000
[ 57.149735] Internal error: Oops: 817 [#1] ARM
[ 57.154402] Modules linked in: musb_dsps musb_hdrc pvrsrvkm(O) cryptodev(O) musb_am335x libcomposite configfs
[ 57.164895] CPU: 0 PID: 1628 Comm: test-pwm Tainted: G O 3.14.26-g2489c02-dirty #274
[ 57.173944] task: cf7b3400 ti: cf7f8000 task.ti: cf7f8000
[ 57.179641] PC is at pwm_ecap_get_rpm_show+0x68/0x94
[ 57.184878] LR is at wake_up_klogd+0x3c/0x48
[ 57.189370] pc : [<c02930e8>] lr : [<c00623a0>] psr: 000f0013
[ 57.189370] sp : cf7f9e40 ip : cf7f9d60 fp : cf7f9e5c
[ 57.201419] r10: c05fc53c r9 : cf4e1000 r8 : 00001000
[ 57.206906] r7 : 00000fff r6 : cf074a00 r5 : cf2421c0 r4 : cf4e1000
[ 57.213760] r3 : 00000000 r2 : 00000000 r1 : 00000000 r0 : c07497a8
[ 57.220619] Flags: nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 57.228112] Control: 10c5387d Table: 8c480019 DAC: 00000015
[ 57.234147] Process test-pwm (pid: 1628, stack limit = 0xcf7f8238)
[ 57.240650] Stack: (0xcf7f9e40 to 0xcf7fa000)
[ 57.245242] 9e40: 00000000 cf000400 cf5ae080 c083971c cf7f9e74 cf7f9e60 c035af08 c029308c
[ 57.253840] 9e60: cf5ae080 cf50b008 cf7f9ea4 cf7f9e78 c0126f24 c035aef0 c0126e90 cf074a00
[ 57.262440] 9e80: 00000001 cf5ae080 cf7f9ec8 cc3ccc80 00000000 00000001 cf7f9eb4 cf7f9ea8
[ 57.271042] 9ea0: c0129cdc c0126e9c cf7f9f04 cf7f9eb8 c00e92bc c0129cbc cf5ae0b0 00010650
[ 57.279636] 9ec0: 00000004 cf7f9f78 00000000 00000000 cf7f9f04 cf7f9ee0 c022e4c4 cf074a00
[ 57.288236] 9ee0: 00000004 00010650 cf7f9f78 00000004 00000004 00010650 cf7f9f44 cf7f9f08
[ 57.296834] 9f00: c012a65c c00e9100 00000001 00000002 00000000 00000000 c005dc6c cc3ccc80
[ 57.305432] 9f20: 00000004 00010650 cf7f9f78 00000004 cf7f8000 00010650 cf7f9f74 cf7f9f48
[ 57.314033] 9f40: c00cb748 c012a554 c00e3734 c00e36b4 00000000 00000000 cc3ccc80 cc3ccc80
[ 57.322630] 9f60: 00000004 00010650 cf7f9fa4 cf7f9f78 c00cb920 c00cb6bc 00000000 00000000
[ 57.331226] 9f80: 00000000 beb15c98 00008355 00000003 c000e964 00000000 00000000 cf7f9fa8
[ 57.339822] 9fa0: c000e7e0 c00cb8e8 00000000 beb15c98 00000003 00010650 00000004 00000001
[ 57.348422] 9fc0: 00000000 beb15c98 00008355 00000003 00000000 00000000 46f17000 00000000
[ 57.357024] 9fe0: 00000000 beb15c74 00008469 470665bc 40000010 00000003 00000000 00000000
[ 57.365603] Backtrace:
[ 57.368224] [<c0293080>] (pwm_ecap_get_rpm_show) from [<c035af08>] (dev_attr_show+0x24/0x50)
[ 57.377077] r5:c083971c r4:cf5ae080
[ 57.380875] [<c035aee4>] (dev_attr_show) from [<c0126f24>] (sysfs_kf_seq_show+0x94/0x110)
[ 57.389453] r5:cf50b008 r4:cf5ae080
[ 57.393250] [<c0126e90>] (sysfs_kf_seq_show) from [<c0129cdc>] (kernfs_seq_show+0x2c/0x30)
[ 57.401923] r10:00000001 r9:00000000 r8:cc3ccc80 r7:cf7f9ec8 r6:cf5ae080 r5:00000001
[ 57.410190] r4:cf074a00 r3:c0126e90
[ 57.413988] [<c0129cb0>] (kernfs_seq_show) from [<c00e92bc>] (seq_read+0x1c8/0x4a0)
[ 57.422039] [<c00e90f4>] (seq_read) from [<c012a65c>] (kernfs_fop_read+0x114/0x15c)
[ 57.430080] r10:00010650 r9:00000004 r8:00000004 r7:cf7f9f78 r6:00010650 r5:00000004
[ 57.438346] r4:cf074a00
[ 57.441047] [<c012a548>] (kernfs_fop_read) from [<c00cb748>] (vfs_read+0x98/0x138)
[ 57.448995] r10:00010650 r9:cf7f8000 r8:00000004 r7:cf7f9f78 r6:00010650 r5:00000004
[ 57.457257] r4:cc3ccc80
[ 57.459945] [<c00cb6b0>] (vfs_read) from [<c00cb920>] (SyS_read+0x44/0x90)
[ 57.467167] r10:00010650 r8:00000004 r7:cc3ccc80 r6:cc3ccc80 r5:00000000 r4:00000000
[ 57.475464] [<c00cb8dc>] (SyS_read) from [<c000e7e0>] (ret_fast_syscall+0x0/0x30)
[ 57.483316] r10:00000000 r8:c000e964 r7:00000003 r6:00008355 r5:beb15c98 r4:00000000
[ 57.491594] Code: e5942000 e30907a8 e5953020 e34c0074 (e5832000)
[ 57.498103] ---[ end trace 9e3da6e7e3eecd69 ]---
Segmentation fault
root@am335x-evm:/usr#
here we are getting --why we are getting kernel panic -
printk(KERN_INFO "get:value:%x %x %x %x\n",buf[0],buf[1],buf[2],buf[3]); //till here we are getting fine
memcpy((char *)pwm->rpm,buf,4); // from here kernel panic we are getting
printk(KERN_INFO "sys:get:value:rpm:%d \n",pwm->rpm);
please help us here -- if i am doing anything wrong -- ?? how to send the data from kernel space to userspace.
regards,
Viswanath K