This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with weston display

Other Parts Discussed in Thread: AM5728

Dear All,

We are working on the custom H/W designed with AM5728. We have interfaced the LCD and we are able to run the kmscube.whereas while working with weston we are facing the following issues. Can any help on this point. Please find the following messages,

am57xx-evm login: root
root@am57xx-evm:~# weston
Date: 2015-10-07 UTC
[20:04:06.977] weston 1.6.0
               wayland.freedesktop.org/
               Bug reports to: bugs.freedesktop.org/enter_bug.cgi
               Build: 1.5.93-5-g2858cc2 configure.ac: bump version to 1.6.0 (2014-09-19 13:40:14 +0300)
[20:04:06.977] OS: Linux, 4.1.6-g52c4aa7, #1 SMP PREEMPT Wed Oct 7 14:52:06 EDT 2015, armv7l
[20:04:06.977] Using config file '/etc//weston.ini'
[20:04:06.977] Loading module '/usr/lib/weston/wayland-backend.so'
[20:04:06.978] Failed to load module: /usr/lib/weston/wayland-backend.so: cannot open shared object file: No such file or directory

root@am57xx-evm:/usr/bin# ./weston-fullscreen
failed to connect to Wayland display: No such file or directory
failed to create display: No such file or directory
root@am57xx-evm:/usr/bin#

root@am57xx-evm:/usr/bin# weston-calibrator
failed to connect to Wayland display: No such file or directory
failed to create display: No such file or directory
root@am57xx-evm:/usr/bin# kmscube
trying to load module omapdrm...success.
### Display [0]: CRTC = 28, Connector = 26
        Mode chosen [1280x800] : Clock => 69300, Vertical refresh => 60, Type => 72
        Horizontal => 1280, 1328, 1360, 1404, 0
        Vertical => 800, 804, 811, 823, 0
### Primary display => ConnectorId = 26, Resolution = 1280x800
failed to load module: /usr/lib/gbm/gbm_dri.so: cannot open shared object file: No such file or directory
failed to load module: /usr/lib/gbm/gbm_gallium_drm.so: cannot open shared object file: No such file or directory
loaded module: gbm_pvr.so
PVR:(Warning): PVRSRVOpenDCDevice: Warning - 138 returned [80, /bridged_pvr_dc_glue.c]
Using display 0x1 with EGL version 1.4
EGL Version "1.4 build 1.9@2253347"
EGL Vendor "Imagination Technologies"
EGL Extensions "EGL_IMG_client_api_ogl EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cu"
^C
Handling signal number = 2
Cleanup of GL, GBM and DRM completed
root@am57xx-evm:/usr/bin#


Thanks & Regards,

N.V.Subbaih