This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can not set EHRPWM in am335x in uboot

Hi there

 

We want to use ehrpwm1 to dim the LED indicator except ecap for LCD backlight.

We want it start in very beginning, so we put it in uboot.

We check the document TRM.

 

We try to add the code in the file board/siemens/pxm2/board.c of u-boot.

static int enable_pwm(void)

{

        struct pwmss_regs *pwmss = (struct pwmss_regs *)PWMSS0_BASE;

        struct pwmss_ecap_regs *ecap;

        int ticks = PWM_TICKS;

        int duty = PWM_DUTY;

#ifdef LED_PWM

        struct pwmss_regs *pwmss1 = (struct pwmss_regs *)PWMSS1_BASE;

        struct pwmss_epwm_regs *epwm;

#endif

 

        ecap = (struct pwmss_ecap_regs *)AM33XX_ECAP0_BASE;

        /* enable clock */

        setbits_le32(&pwmss->clkconfig, ECAP_CLK_EN);

        /* TimeStam Counter register */

        writel(0xdb9, &ecap->tsctr);

        /* config period */

        writel(ticks - 1, &ecap->cap3);

        writel(ticks - 1, &ecap->cap1);

        setbits_le16(&ecap->ecctl2,

                     (ECTRL2_MDSL_ECAP | ECTRL2_SYNCOSEL_MASK | 0xd0));

        /* config duty */

        writel(duty, &ecap->cap2);

        writel(duty, &ecap->cap4);

        /* start */

        setbits_le16(&ecap->ecctl2, ECTRL2_CTRSTP_FREERUN);

 

#ifdef LED_PWM    /* ehrpwm1A */

        epwm = (struct pwmss_epwm_regs *)AM33XX_EPWM1_BASE;

        /* enable clock */

    setbits_le32(&pwmss1->clkconfig, EPWM_CLK_EN);

#if 0

        setbits_le16(&epwm->tbprd, 1200);

//     setbits_le16(&epwm->tbctl, TBCTL_SYNCOSEL);

//     setbits_le16(&epwm->aqctla, ((1<<2)|(2<<4)));

#else

    writel(0, &epwm->tbctl);

//     writel(1200<<16, &epwm->tbprd);

//     writew(TBCTL_SYNCOSEL, &epwm->tbctl);

//     writew(((1<<2)|(2<<4)), &epwm->aqctla);

#endif

#endif

        return 0;

}

 

When we try to write the register after 0x48302200(AM33XX_EPWM1_BASE)

It shows below and reset again.

 

U-Boot SPL 2013.10-00198-gb348f87-dirty (Feb 18 2016 - 23:33:42)

reading u-boot.img

reading u-boot.img

 

 

U-Boot 2013.10-00198-gb348f87-dirty (Feb 18 2016 - 23:33:42)

 

I2C:   ready

DRAM:  512 MiB

data abort

 

    MAYBE you should read doc/README.arm-unaligned-accesses

 

pc : [<9ff84c80>]          lr : [<9ff84c24>]

sp : 9ef49ee8  ip : 00000045     fp : 80100020

r10: 80111d7c  r9 : 9ef49f30     r8 : 4030cdcc

r7 : 4030cb7c  r6 : 00000002     r5 : 00028bd0  r4 : 00000000

r3 : 48302000  r2 : 0000012a     r1 : 000002d6  r0 : 0000006f

Flags: nzCv  IRQs off  FIQs on  Mode SVC_32

Resetting CPU ...

 

resetting ...

 

U-Boot SPL 2013.10-00198-gb348f87-dirty (Feb 18 2016 - 23:33:42)

reading u-boot.img

reading u-boot.img

 

We use U-Boot 2013.10, do you have any idea ?

Wich