This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Toshiba BENAND ( TC58BVG1S3HBAI4 24nm 2Gbit BENAND 3.3V 2KB page sizeBuilt-in ECC NAND) support

Hi All

We have a custom board with DM368 and ipnc rdk 5.1 reference code. We like to use  Toshiba BENAND (Built-in ECC NAND). The custom board is in NAND boot mode. Is this part is supported by RBL (Because of built-in hardware ECC ) ?. What changes are need to be done for support in u-boot and kernel.