Hello,
when I'm reading the "XDC Consumers User Guide" (spruex4.pdf) to better understand, what the XDC tools are, there is a section 1.6.1 "Using the CDOC Reference Help System" with the command "xs xdc.tools.cdoc.sg". When I run this command, I get the following error message:
warning: package xdc.tools.sg.linux_swt depends on the Mozilla browser for some functionality. Your environment doesn't currently point to Mozilla, so some XDC graphical tools may fail. To prevent this, please set up the following in your environment:
- set the MOZILLA_FIVE_HOME environment variable. Its value should be the directory that contains the file run-mozilla.sh, which you can find using the command
locate run-mozilla.sh
I created the variable MOZILLA_FIVE_HOME that consists the directory of run-mozilla.sh and created another variable LD_LIBRARY_PATH which includes the MOZILLA_FIVE_HOME var and the MOZILLA_FIVE_HOME/plugins directory. But the command again says that my environment doesn't point to mozilla. So I can't use the CDOC viewer. Does anybody has an idea what I do wrong? I'm using Fedora 12 with DVSDK 3.10.00.16, XDC-tools 3.16.01.27, Firefox 3.5 and Eclipse 3.5.1.
Thanks for any help!