Part Number: TMDSICE3359
Tool/software: Linux
Hello,
I am trying to set up the Processor SDK linux in TMDSICE3359. Previously I was working in Processor SDK for AM335X , the main reason for moving into the Processor SDK Linux because of the dual MAC functionality in linux environment. Now I am following this link " processors.wiki.ti.com/.../Processor_SDK_Linux_Setup_Script" to setup the Linux SDK on ICE_V2_BOARD. Just a background about exactly I am doing so that it will easier to understand the use case. With one of the ethernet port we are running the EtherCAT functionality using acontis Ethercat Master and on another ethernet port we will run the simple ethernet application to accept the TCP packets from the host PC (basically from Android application). There are few doubts which I am having in setting up the Processor SDK Linux.These doubts are simpler for those who already have setup this , but I am facing since it is my first time.
1. In the point 4. Configure your development environment in the above link the ethernet connection is shown in the diagram . What is the purpose of this ethernet connection is it really necessary?
In the setup.sh script in the uboot setup if I am choosing to put the kernel and file system in the sd card and not on tftp to build, then I think ethernet connect won't be required?
2. In the linux processor SDK, where is the compiler is located to build the ARM applications on "TMDSICE3359" ? I mean to say the path of the compiler?
3. Last question is , can you please tell me the example ethernet application in Processor SDK Linux which I can use to send and receive the TCP packets?
I will be very grateful if somebody can help me as soon as possible.
Thanks and Regards,
Mohit