Part Number: AM5728
Other Parts Discussed in Thread: TMDSEVM572X, TMDSCM572X,
Tool/software: Linux
Hello,
I have TMDSEVM572X and TMDSCM572X(camera module) and use PSDK v3.2.0.5.
When I run the camera application as below, Qt window starts up on the LCD, but the capture image of the camera module is not displayed. Then the following error is displayed on the console. Please let me know if you have some advice to me.
root@am57xx-evm:~# /usr/share/qt5/examples/multimediawidgets/camera/camera
Using Wayland-EGL
wlpvr: PVR Services Initialised
Unable to query the parameter info: "Invalid argument"
Unable to query the parameter info: "Invalid argument"
Unable to query the parameter info: "Invalid argument"
Unable to query the parameter info: "Invalid argument"
Unable to query the parameter info: "Invalid argument"
Unable to query the parameter info: "Invalid argument"
[ 365.449195] vip 48990000.vip: dma_alloc_coherent of size 12582912 failed
CameraBin error: "Failed to allocate required memory."
CameraBin error: "Internal data flow error."
When I push icons of Matrix GUI, the capture image of the camera module is displayed correctly on the LCD, so the camera module is fine.
Camera -> Dual Camera Demo -> Run
Also, if I remove the camera module and connect USB camera, the camera application runs correctly and the capture image of USB camera is displayed on the LCD.
root@am57xx-evm:~# /usr/share/qt5/examples/multimediawidgets/camera/camera
[ 57.986264] usb 1-1.1: reset high-speed USB device number 3 using xhci-hcd
Using Wayland-EGL
wlpvr: PVR Services Initialised
Regards,
Kazu