Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hello,
I am using latest TI SDK Linux-4.4.41 with AM335x EVM-SK board.I tested user hello world application with older linux kernel v3.2 but some drivers are not present in this sdk. So I shifted to XXX SDK. after that i cross-compiled kernel source code as per standard procedure and build uImage. but after executing u-boot it hangs at following location
## Booting kernel from Legacy Image at 80100000 ... Image Name: Linux-4.4.41 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3982032 Bytes = 3.8 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ...
I also referred TI wikis link http://processors.wiki.ti.com/index.php/Kernel_-_Common_Problems_Booting_Linux