Part Number: AM5728
Tool/software: Linux
Hello, I'm wondering if anyone can enlighten me as to why my U-Boot fails to debug. I've been following the U-Boot guide: 
and while my SPL works as intended, U-Boot will get stuck immediately upon running. U-Boot loads to the correct RAM address, 0x80800000, has viewable memory in the CCS debugger, and scoping the power rails for our RAM chips shows action during the end stages of the SPL, which to the best of our knowledge indicates the relocation that happens at the end of the SPL occurs.
However, when U-Boot is loaded via JTAG and run, even with DEBUG defined, no messages appear on the serial console, and since there are no programming symbols, it is impossible to tell where the program crashes. Any ideas? This is a rather large blocker for us, and it's got me stumped.
ADDENUM: I know that I have a similar post here:
but I've reached a wall with this, and I just need a nudge in the proper direction.