Part Number: AM5728
Other Parts Discussed in Thread: DP83822HF, DP83849IF,
Tool/software: Linux
Hi.
I'm using AM572x custom board
and, DP 83822HF is connected to RPU2 ETH0/ETH1
DP83822HF Phy chip is used in two Fx modes.
But there is a problem.
The problem is that two ports can not communicate at the same time.
1. B port is not used when A port is used, and there is no reverse case.
2. If you disconnect the A port and connect to the B port, communication can not be performed.
this is phy chip regster log
==== DP83822HF_config_intr 246===
BMCR(0x0): 0x2100
BMSR(0x1): 0x784d
BMSR(0x1): 0x784d
PHYIDR1(0x2): 0x2000
PHYIDR2(0x3): 0xa240
CR1(0x9): 0x0
CR2(0xa): 0x4100
FLDSTS(0xF): 0x0
PHYSTS(0x10): 0x205
PHYSCR(0x11): 0x109
RCSR(0x17): 0x41
LEDCR(0x18): 0x400
PHYCR(0x19): 0x21
GENCFG(0x465): 0xff00
=================
this is schematic
Best Regards,
John Kim