This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BeagleBone Bare Metal PWM driver

Other Parts Discussed in Thread: SYSCONFIG

Hi again Dean. OK, I finally finished cleaning up the PWM bare metal driver for the Beaglebone Black. 
I did PWM output for ehrpwm0/1/2 channels A & B. So it will give you 6 programmable pwm channels
at your desired period and duty cycle. It is about 500 lines and includes baremetal gpio & pinmux . 
Hackaway.............

//
// pwmx.c
//
// pwm test application - 50Hz varying duty cycle for RC-servo control
// activate ehrpwm0A (pin P9_31), ehrpwm0B (pin P9_29), 
// ehrpwm1A (pin P9_14), ehrpwm1B (pin P9_16)
// ehrpwm2A (pin P8_19), ehrpwm2B (pin P8_13)
// also blinks LED USR2 - GPIO1[23]
//
#include "bbbpwm.h"
//
// local functions
//
void GPIOModuleEnab(unsigned int baseAdd) {
if(baseAdd == SOC_GPIO_1_REGS) {
// write to MODULEMODE field of CM_PER_GPIO1_CLKCTRL reg
HWREG(SOC_CM_PER_REGS + CM_PER_GPIO1_CLKCTRL) |= CM_PER_GPIO1_CLKCTRL_MODULEMODE_ENABLE;
// wait for MODULEMODE field to attain value
while(CM_PER_GPIO1_CLKCTRL_MODULEMODE_ENABLE !=
(HWREG(SOC_CM_PER_REGS + CM_PER_GPIO1_CLKCTRL) &
CM_PER_GPIO1_CLKCTRL_MODULEMODE));
// write to OPTFCLKEN_GPIO_1_GDBCLK bit in CM_PER_GPIO1_CLKCTRL
HWREG(SOC_CM_PER_REGS + CM_PER_GPIO1_CLKCTRL) |=
CM_PER_GPIO1_CLKCTRL_OPTFCLKEN_GPIO_1_GDBCLK;
// wait for OPTFCLKEN_GPIO_1_GDBCLK bit to attain value
while(CM_PER_GPIO1_CLKCTRL_OPTFCLKEN_GPIO_1_GDBCLK !=
(HWREG(SOC_CM_PER_REGS + CM_PER_GPIO1_CLKCTRL) &
CM_PER_GPIO1_CLKCTRL_OPTFCLKEN_GPIO_1_GDBCLK));
// wait for IDLEST field in CM_PER_GPIO1_CLKCTRL register to attain value
while((CM_PER_GPIO1_CLKCTRL_IDLEST_FUNC <<
CM_PER_GPIO1_CLKCTRL_IDLEST_SHIFT) !=
(HWREG(SOC_CM_PER_REGS + CM_PER_GPIO1_CLKCTRL) &
CM_PER_GPIO1_CLKCTRL_IDLEST));
// wait for CLKACTIVITY_GPIO_1_GDBCLK bit in CM_PER_L4LS_CLKSTCTRL reg to attain value
while(CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_GPIO_1_GDBCLK !=
(HWREG(SOC_CM_PER_REGS + CM_PER_L4LS_CLKSTCTRL) &
CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_GPIO_1_GDBCLK));
}
// clear DISABLEMODULE bit in CTRL register (enab the module)
HWREG(baseAdd + GPIO_CTRL) &= ~(GPIO_CTRL_DISABLEMODULE);
// set SOFTRESET bit in System Configuration reg
HWREG(baseAdd + GPIO_SYSCONFIG) |= (GPIO_SYSCONFIG_SOFTRESET);
// wait until GPIO Module is reset
while(!(HWREG(baseAdd + GPIO_SYSSTATUS) & GPIO_SYSSTATUS_RESETDONE));
}
void GPIODirectionSet(unsigned int baseAdd, unsigned int pinNo, unsigned int pinDir) {
// check if pin is to be an output
if(GPIO_DIR_OUTPUT == pinDir) {
HWREG(baseAdd + GPIO_OE) &= ~(1 << pinNo);
} else {
HWREG(baseAdd + GPIO_OE) |= (1 << pinNo);
}
}
void GPIOPinWrite(unsigned int baseAdd, unsigned int pinNo, unsigned int pinValue) {
if(pinValue == 1) {
HWREG(baseAdd + GPIO_SETDATAOUT) = (1 << pinNo);
} else {
HWREG(baseAdd + GPIO_CLEARDATAOUT) = (1 << pinNo);
}
}
//
// simple PinMux setup
//
// GPIOaddr - GPIO address from pin_mux.h (and Mode7 column of Header Table in BBB_SRM)
// modeValue - select mode 0 to 7
//
void GPIOPinMuxSetup(unsigned int GPIOaddr, unsigned int modeValue) {
HWREG(SOC_CONTROL_REGS + GPIOaddr) = (modeValue);
}
//
// set clock divider of time-based clock
//
// see TBCTL register in TRM
//
// prescale - time-based clock prescale value 
// choose a value = 14 * X (X = 1,2,4,8...128)
//
void PWMTBClkDiv(unsigned int baseAddr, unsigned int prescale) {
unsigned int clkDiv = prescale;
unsigned int hspClkDiv;
unsigned int lspClkDiv, lspClkDivSetting = 0;
if(clkDiv > EHRPWM_TBCTL_HSPCLKDIV_14) { // 0xE
hspClkDiv = EHRPWM_TBCTL_HSPCLKDIV_DIVBY14; // 0x7
lspClkDiv = clkDiv/EHRPWM_TBCTL_HSPCLKDIV_14; 
while(lspClkDiv > 1) {
lspClkDiv = lspClkDiv >> 1;
lspClkDivSetting++;
}
} else {
hspClkDiv = clkDiv/2;
lspClkDivSetting = EHRPWM_TBCTL_HSPCLKDIV_DIVBY1; // divide by 1
}
HWREGH(baseAddr + EHRPWM_TBCTL) = (HWREGH(baseAddr + EHRPWM_TBCTL) &
(~EHRPWM_TBCTL_CLKDIV)) | ((lspClkDivSetting <<
EHRPWM_TBCTL_CLKDIV_SHIFT) & EHRPWM_TBCTL_CLKDIV);
HWREGH(baseAddr + EHRPWM_TBCTL) = (HWREGH(baseAddr + EHRPWM_TBCTL) &
(~EHRPWM_TBCTL_HSPCLKDIV)) | ((hspClkDiv <<
EHRPWM_TBCTL_HSPCLKDIV_SHIFT) & EHRPWM_TBCTL_HSPCLKDIV);
}
//
// set PWM output period (time-based clock period)
//
// see TBPRD register in TRM
//
// pwmPeriod - desired output pwm period in milliseconds 
// eg pwmPeriod = 20 will yield an output frequency of 50Hz
//
void PWMPeriodSet(unsigned int baseAddr, unsigned int pwmPeriod) {
unsigned int tbPeriod = pwmPeriod*TICKS_PER_MS;
unsigned int counterDir = EHRPWM_COUNT_UP;
char enableShadowWrite = EHRPWM_SHADOW_WRITE_ENABLE;
HWREGH(baseAddr + EHRPWM_TBCTL) = (HWREGH(baseAddr + EHRPWM_TBCTL) &
(~EHRPWM_PRD_LOAD_SHADOW_MASK)) | ((enableShadowWrite <<
EHRPWM_TBCTL_PRDLD_SHIFT) & EHRPWM_PRD_LOAD_SHADOW_MASK);
HWREGH(baseAddr + EHRPWM_TBCTL) = (HWREGH(baseAddr + EHRPWM_TBCTL) &
(~EHRPWM_COUNTER_MODE_MASK)) | ((counterDir <<
EHRPWM_TBCTL_CTRMODE_SHIFT) & EHRPWM_COUNTER_MODE_MASK);
if(EHRPWM_COUNT_UP_DOWN == counterDir) {
HWREGH(baseAddr + EHRPWM_TBPRD) = (unsigned short)tbPeriod/2;
} else {
HWREGH(baseAddr + EHRPWM_TBPRD) = (unsigned short)tbPeriod;
}
}
//
// load counter compare register A
//
// CMPAVal must be less than TBPRD
// see Counter-Compare Submodule in TRM
//
// this will hang the mpu if u try to load a 
// pwm module that has NOT been initialized
//
char PWMLoadCMPA(unsigned int baseAddr, unsigned int CMPAVal) {
char enableShadowWrite = EHRPWM_SHADOW_WRITE_ENABLE;
unsigned int ShadowToActiveLoadTrigger = EHRPWM_COMPA_LOAD_COUNT_EQUAL_ZERO_OR_PERIOD;
char OverwriteShadowFull = EHRPWM_CMPCTL_OVERWR_SH_FL;
char status = FALSE;
if((OverwriteShadowFull) || ((HWREGH(baseAddr+EHRPWM_CMPCTL) & EHRPWM_CMPCTL_SHDWAFULL) 
== EHRPWM_SHADOW_A_EMPTY)) {
HWREGH(baseAddr + EHRPWM_CMPCTL) = (HWREGH(baseAddr + EHRPWM_CMPCTL) &
(~EHRPWM_CMPCTL_SHDWAMODE)) | ((enableShadowWrite <<
EHRPWM_CMPCTL_SHDWAMODE_SHIFT) & EHRPWM_CMPCTL_SHDWAMODE);
HWREGH(baseAddr + EHRPWM_CMPCTL) = (HWREGH(baseAddr + EHRPWM_CMPCTL) &
(~EHRPWM_COMPA_LOAD_MASK)) |((ShadowToActiveLoadTrigger <<
EHRPWM_CMPCTL_LOADAMODE_SHIFT) & EHRPWM_COMPA_LOAD_MASK);
HWREGH(baseAddr + EHRPWM_CMPA) = CMPAVal & EHRPWM_CMPA_CMPA;
status = TRUE;
}
return status;
}
//
// load counter compare register B
//
// CMPBVal must be less than TBPRD
// see Counter-Compare Submodule in TRM
//
char PWMLoadCMPB(unsigned int baseAddr, unsigned int CMPBVal) {
char enableShadowWrite = EHRPWM_SHADOW_WRITE_ENABLE;
unsigned int ShadowToActiveLoadTrigger = EHRPWM_COMPB_LOAD_COUNT_EQUAL_ZERO_OR_PERIOD;
char OverwriteShadowFull = EHRPWM_CMPCTL_OVERWR_SH_FL;
char status = FALSE;
if((OverwriteShadowFull) || ((HWREGH(baseAddr+EHRPWM_CMPCTL) & EHRPWM_CMPCTL_SHDWBFULL) 
== EHRPWM_SHADOW_B_EMPTY)) {
HWREGH(baseAddr + EHRPWM_CMPCTL) = (HWREGH(baseAddr + EHRPWM_CMPCTL) &
(~EHRPWM_CMPCTL_SHDWBMODE)) | ((enableShadowWrite <<
EHRPWM_CMPCTL_SHDWBMODE_SHIFT) & EHRPWM_CMPCTL_SHDWBMODE);
HWREGH(baseAddr + EHRPWM_CMPCTL) = (HWREGH(baseAddr + EHRPWM_CMPCTL) &
(~EHRPWM_COMPB_LOAD_MASK)) |((ShadowToActiveLoadTrigger <<
EHRPWM_CMPCTL_LOADBMODE_SHIFT) & EHRPWM_COMPB_LOAD_MASK);
HWREGH(baseAddr + EHRPWM_CMPB) = CMPBVal & EHRPWM_CMPB_CMPB;
status = TRUE;
}
return status;
}
void PWMconfigAQActionOnA(unsigned int baseAddr,
unsigned int zero,
unsigned int period,
unsigned int CAUp,
unsigned int CADown,
unsigned int CBUp,
unsigned int CBDown,
unsigned int SWForced) {
HWREGH(baseAddr + EHRPWM_AQCTLA) =
((CBDown << EHRPWM_AQCTLA_CBD_SHIFT) & EHRPWM_AQCTLA_CBD) |
((CBUp << EHRPWM_AQCTLA_CBU_SHIFT) & EHRPWM_AQCTLA_CBU) |
((CADown << EHRPWM_AQCTLA_CAD_SHIFT) & EHRPWM_AQCTLA_CAD) |
((CAUp << EHRPWM_AQCTLA_CAU_SHIFT) & EHRPWM_AQCTLA_CAU) |
((period << EHRPWM_AQCTLA_PRD_SHIFT) & EHRPWM_AQCTLA_PRD) |
((zero << EHRPWM_AQCTLA_ZRO_SHIFT) & EHRPWM_AQCTLA_ZRO);
HWREGH(baseAddr + EHRPWM_AQSFRC) = (HWREGH(baseAddr + EHRPWM_AQSFRC) &
(~EHRPWM_AQSFRC_ACTSFA)) | ((SWForced <<
EHRPWM_AQSFRC_ACTSFA_SHIFT) & EHRPWM_AQSFRC_ACTSFA);
}
void PWMconfigAQActionOnB(unsigned int baseAddr,
unsigned int zero,
unsigned int period,
unsigned int CAUp,
unsigned int CADown,
unsigned int CBUp,
unsigned int CBDown,
unsigned int SWForced) {
HWREGH(baseAddr + EHRPWM_AQCTLB) =
((CBDown << EHRPWM_AQCTLB_CBD_SHIFT) & EHRPWM_AQCTLB_CBD) |
((CBUp << EHRPWM_AQCTLB_CBU_SHIFT) & EHRPWM_AQCTLB_CBU) |
((CADown << EHRPWM_AQCTLB_CAD_SHIFT) & EHRPWM_AQCTLB_CAD) |
((CAUp << EHRPWM_AQCTLB_CAU_SHIFT) & EHRPWM_AQCTLB_CAU) |
((period << EHRPWM_AQCTLB_PRD_SHIFT) & EHRPWM_AQCTLB_PRD) |
((zero << EHRPWM_AQCTLB_ZRO_SHIFT) & EHRPWM_AQCTLB_ZRO);
HWREGH(baseAddr + EHRPWM_AQSFRC) =
(HWREGH(baseAddr + EHRPWM_AQSFRC) & (~EHRPWM_AQSFRC_ACTSFB)) |
((SWForced << EHRPWM_AQSFRC_ACTSFB_SHIFT) & EHRPWM_AQSFRC_ACTSFB);
}
//
// heavily hacked config code from rodrigo in brazil
//
// pwmx: bit1-pwm0, bit2-pwm1, bit3-pwm2 (0-disable or 1-enable PWM module X)
// pwmPeriod: period of pwm output in msec
//
void PWMconfig(unsigned int pwmx, unsigned int pwmPeriod) {
// config L3_PER and L4_PER clocks
HWREG(SOC_PRCM_REGS + CM_PER_L3S_CLKSTCTRL) |= CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_PRCM_REGS + CM_PER_L3S_CLKSTCTRL) & 
CM_PER_L3S_CLKSTCTRL_CLKTRCTRL) != CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_PRCM_REGS + CM_PER_L3_CLKSTCTRL) |= CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_PRCM_REGS + CM_PER_L3_CLKSTCTRL) & 
CM_PER_L3_CLKSTCTRL_CLKTRCTRL) != CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_PRCM_REGS + CM_PER_L3_INSTR_CLKCTRL) |= 
CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE;
while((HWREG(SOC_PRCM_REGS + CM_PER_L3_INSTR_CLKCTRL) & 
CM_PER_L3_INSTR_CLKCTRL_MODULEMODE) != CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE);
HWREG(SOC_PRCM_REGS + CM_PER_L3_CLKCTRL) |= CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE;
while((HWREG(SOC_PRCM_REGS + CM_PER_L3_CLKCTRL) & 
CM_PER_L3_CLKCTRL_MODULEMODE) != CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE);
HWREG(SOC_PRCM_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) |= 
CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_PRCM_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) & 
CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL) != CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_PRCM_REGS + CM_PER_L4LS_CLKSTCTRL) |= CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_PRCM_REGS + CM_PER_L4LS_CLKSTCTRL) & 
CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL) != CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_PRCM_REGS + CM_PER_L4LS_CLKCTRL) |= CM_PER_L4LS_CLKCTRL_MODULEMODE_ENABLE;
while((HWREG(SOC_PRCM_REGS + CM_PER_L4LS_CLKCTRL) & 
CM_PER_L4LS_CLKCTRL_MODULEMODE) != CM_PER_L4LS_CLKCTRL_MODULEMODE_ENABLE);
if(pwmx & 0x1) { // config EPWMSS0 clock
HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS0_CLKCTRL) |=
CM_PER_EPWMSS0_CLKCTRL_MODULEMODE_ENABLE;
while(CM_PER_EPWMSS0_CLKCTRL_MODULEMODE_ENABLE !=
(HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS0_CLKCTRL) & CM_PER_EPWMSS0_CLKCTRL_MODULEMODE));
while((CM_PER_EPWMSS0_CLKCTRL_IDLEST_FUNC << CM_PER_EPWMSS0_CLKCTRL_IDLEST_SHIFT) !=
(HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS0_CLKCTRL) & CM_PER_EPWMSS0_CLKCTRL_IDLEST));
} 
if(pwmx & 0x2) { // config EPWMSS1 clock
HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS1_CLKCTRL) |=
CM_PER_EPWMSS1_CLKCTRL_MODULEMODE_ENABLE;
while(CM_PER_EPWMSS1_CLKCTRL_MODULEMODE_ENABLE !=
(HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS1_CLKCTRL) & CM_PER_EPWMSS1_CLKCTRL_MODULEMODE));
while((CM_PER_EPWMSS1_CLKCTRL_IDLEST_FUNC << CM_PER_EPWMSS1_CLKCTRL_IDLEST_SHIFT) !=
(HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS1_CLKCTRL) & CM_PER_EPWMSS1_CLKCTRL_IDLEST));
}
if(pwmx & 0x4) { // config EPWMSS2 clock
HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS2_CLKCTRL) |=
CM_PER_EPWMSS2_CLKCTRL_MODULEMODE_ENABLE;
while(CM_PER_EPWMSS2_CLKCTRL_MODULEMODE_ENABLE !=
(HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS2_CLKCTRL) & CM_PER_EPWMSS2_CLKCTRL_MODULEMODE));
while((CM_PER_EPWMSS2_CLKCTRL_IDLEST_FUNC << CM_PER_EPWMSS2_CLKCTRL_IDLEST_SHIFT) !=
(HWREG(SOC_PRCM_REGS + CM_PER_EPWMSS2_CLKCTRL) & CM_PER_EPWMSS2_CLKCTRL_IDLEST));
}
// wait on L3 & L4 clock activity
while(!(HWREG(SOC_PRCM_REGS + CM_PER_L3S_CLKSTCTRL) & 
CM_PER_L3S_CLKSTCTRL_CLKACTIVITY_L3S_GCLK));
while(!(HWREG(SOC_PRCM_REGS + CM_PER_L3_CLKSTCTRL) & 
CM_PER_L3_CLKSTCTRL_CLKACTIVITY_L3_GCLK));
while(!(HWREG(SOC_PRCM_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) & 
(CM_PER_OCPWP_L3_CLKSTCTRL_CLKACTIVITY_OCPWP_L3_GCLK | 
CM_PER_OCPWP_L3_CLKSTCTRL_CLKACTIVITY_OCPWP_L4_GCLK)));
while(!(HWREG(SOC_PRCM_REGS + CM_PER_L4LS_CLKSTCTRL) & 
(CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_L4LS_GCLK )));
if(pwmx & 0x1) { // PWM0
HWREG(SOC_PWMSS0_REGS + PWMSS_CLOCK_CONFIG) |= PWMSS_EHRPWM_CLK_EN_ACK; // enable PWMSSx clocks
HWREG(SOC_CONTROL_REGS + CONTROL_PWMSS_CTRL) |= CONTROL_PWMSS_CTRL_PWMSS0_TBCLKEN; // enable Timer Base Module Clock in Control Module
PWMTBClkDiv(SOC_EPWM_0_REGS, PWM_PRESCALE); // config time-base clock
PWMPeriodSet(SOC_EPWM_0_REGS, pwmPeriod); // config PWM period
PWMconfigAQActionOnA(SOC_EPWM_0_REGS, // config Action Qualifiers for PWM0A
EHRPWM_AQCTLA_ZRO_EPWMXAHIGH, // high when CTR = 0
EHRPWM_AQCTLA_PRD_DONOTHING,
EHRPWM_AQCTLA_CAU_EPWMXALOW, // low when CTR = CMPA
EHRPWM_AQCTLA_CAD_DONOTHING,
EHRPWM_AQCTLA_CBU_DONOTHING,
EHRPWM_AQCTLA_CBD_DONOTHING,
EHRPWM_AQSFRC_ACTSFA_DONOTHING);
PWMconfigAQActionOnB(SOC_EPWM_0_REGS, // PWM0B
EHRPWM_AQCTLB_ZRO_EPWMXBHIGH, // high when CTR = 0
EHRPWM_AQCTLB_PRD_DONOTHING,
EHRPWM_AQCTLB_CAU_DONOTHING,
EHRPWM_AQCTLB_CAD_DONOTHING,
EHRPWM_AQCTLB_CBU_EPWMXBLOW, // low when CTR = CMPB
EHRPWM_AQCTLB_CBD_DONOTHING,
EHRPWM_AQSFRC_ACTSFB_DONOTHING);
}
if(pwmx & 0x2) { // PWM1
HWREG(SOC_PWMSS1_REGS + PWMSS_CLOCK_CONFIG) |= PWMSS_EHRPWM_CLK_EN_ACK;
HWREG(SOC_CONTROL_REGS + CONTROL_PWMSS_CTRL) |= CONTROL_PWMSS_CTRL_PWMSS1_TBCLKEN;
PWMTBClkDiv(SOC_EPWM_1_REGS, PWM_PRESCALE);
PWMPeriodSet(SOC_EPWM_1_REGS, pwmPeriod);
PWMconfigAQActionOnA(SOC_EPWM_1_REGS, // PWM1A
EHRPWM_AQCTLA_ZRO_EPWMXAHIGH, // high when CTR = 0
EHRPWM_AQCTLA_PRD_DONOTHING,
EHRPWM_AQCTLA_CAU_EPWMXALOW, // low when CTR = CMPA
EHRPWM_AQCTLA_CAD_DONOTHING,
EHRPWM_AQCTLA_CBU_DONOTHING,
EHRPWM_AQCTLA_CBD_DONOTHING,
EHRPWM_AQSFRC_ACTSFA_DONOTHING);
PWMconfigAQActionOnB(SOC_EPWM_1_REGS, // PWM1B
EHRPWM_AQCTLB_ZRO_EPWMXBHIGH, // high when CTR = 0
EHRPWM_AQCTLB_PRD_DONOTHING,
EHRPWM_AQCTLB_CAU_DONOTHING,
EHRPWM_AQCTLB_CAD_DONOTHING,
EHRPWM_AQCTLB_CBU_EPWMXBLOW, // low when CTR = CMPB
EHRPWM_AQCTLB_CBD_DONOTHING,
EHRPWM_AQSFRC_ACTSFB_DONOTHING);
}
if(pwmx & 0x4) { // PWM2
HWREG(SOC_PWMSS2_REGS + PWMSS_CLOCK_CONFIG) |= PWMSS_EHRPWM_CLK_EN_ACK;
HWREG(SOC_CONTROL_REGS + CONTROL_PWMSS_CTRL) |= CONTROL_PWMSS_CTRL_PWMSS2_TBCLKEN;
PWMTBClkDiv(SOC_EPWM_2_REGS, PWM_PRESCALE);
PWMPeriodSet(SOC_EPWM_2_REGS, pwmPeriod);
PWMconfigAQActionOnA(SOC_EPWM_2_REGS, // PWM2A
EHRPWM_AQCTLA_ZRO_EPWMXAHIGH, // high when CTR = 0
EHRPWM_AQCTLA_PRD_DONOTHING,
EHRPWM_AQCTLA_CAU_EPWMXALOW, // low when CTR = CMPA
EHRPWM_AQCTLA_CAD_DONOTHING,
EHRPWM_AQCTLA_CBU_DONOTHING,
EHRPWM_AQCTLA_CBD_DONOTHING,
EHRPWM_AQSFRC_ACTSFA_DONOTHING);
PWMconfigAQActionOnB(SOC_EPWM_2_REGS, // PWM2B
EHRPWM_AQCTLB_ZRO_EPWMXBHIGH, // high when CTR = 0
EHRPWM_AQCTLB_PRD_DONOTHING,
EHRPWM_AQCTLB_CAU_DONOTHING,
EHRPWM_AQCTLB_CAD_DONOTHING,
EHRPWM_AQCTLB_CBU_EPWMXBLOW, // low when CTR = CMPB
EHRPWM_AQCTLB_CBD_DONOTHING,
EHRPWM_AQSFRC_ACTSFB_DONOTHING);
}
return;
}
//
// spin your wheels
//
void Delay(volatile unsigned int count) {
while(count--);
}
//
// main program
//
// move a RC-servo back and forth and watch das-blinken-light!
//
void main() {
unsigned int i, delta, base, direction, tbprd;
GPIOModuleEnab(GPIO_ADDR); // enable GPIO module
GPIODirectionSet(GPIO_ADDR, LED_USR2, GPIO_DIR_OUTPUT); // set GPIO pin as output
GPIOPinMuxSetup(GPIO_1_23, 7); // muxout LED USR2
GPIOPinMuxSetup(GPIO_0_22, 4); // pin P8_19 ehrpwm2A
GPIOPinMuxSetup(GPIO_0_23, 4); // pin P8_13 ehrpwm2B
GPIOPinMuxSetup(GPIO_1_18, 6); // pin P9_14 ehrpwm1A
GPIOPinMuxSetup(GPIO_1_19, 6); // pin P9_16 ehrpwm1B
GPIOPinMuxSetup(GPIO_3_14, 1); // pin P9_31 ehrpwm0A
GPIOPinMuxSetup(GPIO_3_15, 1); // pin P9_29 ehrpwm0B
PWMconfig(0x7, PWM_PERIOD_MS); // config PWM 0, 1, 2
base = (TICKS_PER_MS * PWM_PERIOD_MS)/20; // 1ms base pulse width - RC Servo
delta = base/10; // .1ms pulse width increment
i = 4;
direction = 1;
while(1) {
if(direction == 1) i++;
if(direction == 0) i--;
tbprd = base + (delta * i);
PWMLoadCMPA(SOC_EPWM_0_REGS, tbprd);
PWMLoadCMPB(SOC_EPWM_0_REGS, tbprd); 
PWMLoadCMPA(SOC_EPWM_1_REGS, tbprd);
PWMLoadCMPB(SOC_EPWM_1_REGS, tbprd); 
PWMLoadCMPA(SOC_EPWM_2_REGS, tbprd);
PWMLoadCMPB(SOC_EPWM_2_REGS, tbprd); 
if(i <= 0) direction = 1;
if(i >= 10) direction = 0;
GPIOPinWrite(GPIO_ADDR, LED_USR2, 1);
Delay(0x2FFFF);
GPIOPinWrite(GPIO_ADDR, LED_USR2, 0);
Delay(0x3FFFF);
GPIOPinWrite(GPIO_ADDR, LED_USR2, 1);
Delay(0x1FFFF);
GPIOPinWrite(GPIO_ADDR, LED_USR2, 0);
Delay(0xAFFFF);
}
} 

and the header file bbbpwm.h :

//
// bbbpwm.h - pwm library header file
//
//#include "soc_AM335x.h"
#define SOC_GPIO_1_REGS (0x4804C000)
#define SOC_PWMSS0_REGS (0x48300000)
#define SOC_PWMSS1_REGS (0x48302000)
#define SOC_PWMSS2_REGS (0x48304000)
#define SOC_EPWM_REGS (0x00000200)
#define SOC_EPWM_0_REGS (SOC_PWMSS0_REGS + SOC_EPWM_REGS)
#define SOC_EPWM_1_REGS (SOC_PWMSS1_REGS + SOC_EPWM_REGS)
#define SOC_EPWM_2_REGS (SOC_PWMSS2_REGS + SOC_EPWM_REGS)
#define SOC_ECAP_REGS (0x00000100) // ecap0 not
#define SOC_ECAP_0_REGS (SOC_PWMSS0_REGS + SOC_ECAP_REGS) // implemented
#define SOC_CONTROL_REGS (0x44E10000)
#define SOC_PRCM_REGS (0x44E00000)
#define SOC_CM_PER_REGS (SOC_PRCM_REGS + 0)

//#include "beaglebone.h"
//#include "gpio_v2.h"
#define GPIO_DIR_OUTPUT (GPIO_OE_OUTPUTEN_ENABLED)
#define GPIO_OE_OUTPUTEN_ENABLED (0x0u)
#define GPIO_CTRL (0x130)
#define GPIO_CTRL_DISABLEMODULE (0x00000001u)
#define GPIO_SYSCONFIG (0x10)
#define GPIO_SYSCONFIG_SOFTRESET (0x00000002u)
#define GPIO_SYSSTATUS (0x114)
#define GPIO_SYSSTATUS_RESETDONE (0x00000001u)
#define GPIO_OE (0x134)
#define GPIO_CLEARDATAOUT (0x190)
#define GPIO_SETDATAOUT (0x194)

//#include "hw_control_AM335x.h"
#define CONTROL_PWMSS_CTRL (0x664)
#define CONTROL_PWMSS_CTRL_PWMSS0_TBCLKEN (0x00000001u)
#define CONTROL_PWMSS_CTRL_PWMSS1_TBCLKEN (0x00000002u)
#define CONTROL_PWMSS_CTRL_PWMSS2_TBCLKEN (0x00000004u)

#include "ehrpwm.h" // do not remove, too many defines needed here

//#include "hw_pwmss.h"
#define PWMSS_CLOCK_CONFIG 0x08
#define PWMSS_EHRPWM_CLK_EN_ACK 0x100

//#include "evmAM335x.h"

#include "hw_cm_per.h" // do not remove, too many defines needed here

//#include "interrupt.h"

//#include "hw_types.h"
#define HWREG(x) (*((volatile unsigned int *)(x)))
#define HWREGH(x) (*((volatile unsigned short *)(x)))
#define TRUE 1
#define FALSE 0

//#include "pin_mux.h"
#define GPIO_0_22 (0x0820)
#define GPIO_0_23 (0x0824)
#define GPIO_1_18 (0x0848)
#define GPIO_1_19 (0x084c)
#define GPIO_3_14 (0x0990)
#define GPIO_3_15 (0x0994)
#define GPIO_1_23 (0x085c) // spoof LED USR2
//
// internal macros
//
#define GPIO_ADDR SOC_GPIO_1_REGS // for LED USR2
#define LED_USR2 23 // LED USR2
#define SOC_EHRPWM_1_MODULE_FREQ 100000000 // SYSCLKOUT [10 ns/tick]
#define PWM_PRESCALE 224 // pwm clk divider - TBCLK
#define TICKS_PER_MS 446 // ticks per msec pwm output period
#define PWM_PERIOD_MS 20 // desired pwm output period in ms
// PWM_PRESCALE of 224 = 14 * X (X = 1, 2, 4...128), see TBCTL Register
// TICKS_PER_MS * PWM_PERIOD_MS = period of pwm output in ticks = TBPRD (only 16 bits)
// FINITO

Also, use this command file, from one of the starterware examples. 
I wasted alot of time with flakey-intermittently failing images that weren't linked/built properly. 
None of this is documented for noobs. Copy it into your pwm workspace dir. 

/****************************************************************************/
/* LNK32.CMD - v4.5.0 COMMAND FILE FOR LINKING TMS470 32BIS C/C++ PROGRAMS */
/* */
/* Usage: lnk470 <obj files...> -o <out file> -m <map file> lnk32.cmd */
/* cl470 <src files...> -z -o <out file> -m <map file> lnk32.cmd */
/* */
/* Description: This file is a sample command file that can be used */
/* for linking programs built with the TMS470 C/C++ */
/* Compiler. Use it as a guideline; you may want to change */
/* the allocation scheme according to the size of your */
/* program and the memory layout of your target system. */
/* */
/* Notes: (1) You must specify the directory in which run-time support */
/* library is located. Either add a "-i<directory>" line to */
/* this file, or use the system environment variable C_DIR */
/* to specify a search path for libraries. */
/* */
/* (2) If the run-time support library you are using is not */
/* named below, be sure to use the correct name here. */
/* */
/****************************************************************************/
-stack 0x0008 /* SOFTWARE STACK SIZE */
-heap 0x2000 /* HEAP AREA SIZE */
-e Entry
/* Since we used 'Entry' as the entry-point symbol the compiler issues a */
/* warning (#10063-D: entry-point symbol other than "_c_int00" specified: */
/* "Entry"). The CCS Version (5.1.0.08000) stops building from command */
/* line when there is a warning. So this warning is suppressed with the */
/* below flag. */

--diag_suppress=10063

/* SPECIFY THE SYSTEM MEMORY MAP */

MEMORY
{
DDR_MEM : org = 0x80000000 len = 0x7FFFFFF /* RAM */
}

/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY */

SECTIONS
{
.text:Entry : load > 0x80000000

.text : load > DDR_MEM /* CODE */
.data : load > DDR_MEM /* INITIALIZED GLOBAL AND STATIC VARIABLES */
.bss : load > DDR_MEM /* UNINITIALIZED OR ZERO INITIALIZED */
/* GLOBAL & STATIC VARIABLES */
RUN_START(bss_start)
RUN_END(bss_end)
.const : load > DDR_MEM /* GLOBAL CONSTANTS */
.stack : load > 0x87FFFFF0 /* SOFTWARE SYSTEM STACK */
}

It all looks very large, but this is all self-contained, no hidden functions. 
In CCS/Properties/ARM Linker/File Search Path add only 1 library I could not suss-out:
C:\ti\AM335X_StarterWare_02_00_01_01\binary\armv7a\cgt_ccs\am335x\system_config\Debug\system.lib
You can easily code-in the manifests and eliminate some of the HAL functions to reduce size. 

I encourage others in the bare-metal community to break-out the other subsystems on the bone. 
We can all benefit and build bullet-proof lightning-fast applications. 
The Sitara documentation looks good, but it is a tough cookie. 
I will post UART and MMC/SDcard soon. 

hack-on my brothers!!!!!!!!!!!!!!! dd