Hi I'm trying to run an example of gpio of starterware for BEAGLEBONE. I want to use a delay for the user LEDs. I'm using the library delay.h.and it does not work does nothing. you can help me? thank you very much, the program is as follows .....
#include "soc_AM335x.h"
#include "beaglebone.h"
#include "gpio_v2.h"
#include "interrupt.h"
#include "dmtimer.h"
#include "delay.h"
#define GPIO_INSTANCE_ADDRESS (SOC_GPIO_1_REGS)
#define GPIO_INSTANCE_PIN_NUMBER (23)
int main(void)
{
/* Enabling functional clocks for GPIO1 instance. */
GPIO1ModuleClkConfig();
/* Selecting GPIO1[23] pin for use. */
GPIO1Pin23PinMuxSetup();
/* Enabling the GPIO module. */
GPIOModuleEnable(GPIO_INSTANCE_ADDRESS);
/* Resetting the GPIO module. */
GPIOModuleReset(GPIO_INSTANCE_ADDRESS);
/* Setting the GPIO pin as an output pin. */
GPIODirModeSet(GPIO_INSTANCE_ADDRESS,
GPIO_INSTANCE_PIN_NUMBER,
GPIO_DIR_OUTPUT);
DelayTimerSetup();
while(1)
{
/* Driving a logic HIGH on the GPIO pin. */
GPIOPinWrite(GPIO_INSTANCE_ADDRESS,
GPIO_INSTANCE_PIN_NUMBER,
GPIO_PIN_LOW);
delay(200);
/* Driving a logic LOW on the GPIO pin. */
GPIOPinWrite(GPIO_INSTANCE_ADDRESS,
GPIO_INSTANCE_PIN_NUMBER,
GPIO_PIN_HIGH);
delay(200);
}
}