Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi,
I'm trying to switch my DSP/BIOS + DSPLink application from COFF to EABI because the COFF compiler has some limit on C++ virtual inheritance class size of 0x7FFF bytes (and EABI sets the limit to 0xFFFFFF).
I can compile all my code with the --abi=eabi switch, but I'm having problems with configuration for linking.
My COFF method of linking is to:
1) Run tconf :
/opt/TI/xdctools_3_22_00_09/tconf -Dconfig.importPath="/opt/TI/dspbios_5_41_03_17/packages;/opt/TI/dspbios_5_41_03_17/packages/ti/bios;/opt/TI/dsplink_1_65_00_03/dsplink/dsp/inc/DspBios;/opt/TI/dsplink_1_65_00_03/dsplink/dsp/inc/DspBios/5.XX;.;" -Dconfig.programName="dsp" dsp.tcf 0
2) Compile the generated files.
3) Link my project using the generated dspcfg.cmd linker script.
If I try the same flow with the "--abi-eabi" switch then the compiler throws an error for the "tconf" generated files, e.g.:
" dspcfg.s62", ERROR! at line 2196: [E0200]
Unable to resolve this relocatable expression; relocation support for arbitrary expressions is not available in the C6000 EABI
.word ((:name:$stkptr - :name:$stackname) / STD_TARGWORDMAUS) + 1 ; count
Is there a way to get tconf to generate my EABI linker script like it did for COFF?
I originally asked this question on the compiler tools forum, but I was pointed here with the following suggestion:
As I understand it, you need to use an EABI-friendly version of DSP/BIOS. You probably want to ask this in the DSP/BIOS forum.
Thanks,
Will