Other Parts Discussed in Thread: OMAP-L138
Hello,
we are using the following tools/versions on the ARM side of the OMAP-L138:
- CCS Version 4.2.1.00004
- SYS/BIOS 6.30.03.46
- TMS470 Code Generation Tools 4.6.4
- XDCTOOLS 3.20.07.86
We are interested if it is possible to remove the whole xdc.meta data from the image.
If it is possible, what needs to be done to remove it (at least from the bin resp. the h file generated via AISgen D800K008 Version1.9)?
Currently the following meta data are in the mapfile:
__ASM__
__ISA__
__PLAT__
__TARG__
__TRDR__
I already searched through the forums, but could not find how remove the whole meta data.
One interesting link was:
http://e2e.ti.com/support/development_tools/compiler/f/343/t/85269.aspx?PageIndex=1
However, I could not figure out how to remove the whole meta data for the tools/versions I'm using.
What are the drawbacks if the whole meta data were removed?
Thanks,
Frank