This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Some advice about MMU on the OMAP-L138 and SYSBIOS...



It seems like the MMU module makes several units on the OMAP unaccessable by default. EMIF as an example.

We have a need to access this section to set it up.  Looking for directions how to get the MMU unit and our code to play nice together.

1) We could pull our init code for the EMIF and try to move it into the startup routines in the cfg file.  Doesnt seem to be easy to do with the GUI on CCS.

2) Can we disable the MMU and then call our init routines and then restart the MMU?

3) Build our own MMU routines (not my favorit choise) so that the EMIF is accessable?  Documentation seems to be weak on the attributes like bufferable verses cacheable.

Also it looks like the ARM and the DSP have very different views of the MMU.  We plan to do all the MMU managment on the ARM.  Any issues with that?

Thanks,

 

  • Mike,

    I think you just need to override the default MMU table entry for the EMIF address space.

    Here is an example of how to configure an MMU table entry to allow access to the peripheral memory space beginning at address 0xa0400000:

     var Mmu = xdc.useModule('ti.sysbios.family.arm.arm9.Mmu'); 

    // Force peripheral section to be NON cacheable
    var peripheralAttrs = { type : Mmu.FirstLevelDesc_SECTION, // SECTION descriptor
    bufferable : false, // bufferable
    cacheable : false, // cacheable
    };

     // Define the base address of the 1 Meg page
    // the peripheral resides in.
    var peripheralBaseAddr = 0xa0400000; /* replace with the 1 meg page address of your peripheral */


    // Configure the corresponding MMU page descriptor accordingly
    Mmu.setFirstLevelDescMeta(peripheralBaseAddr, peripheralBaseAddr, peripheralAttrs);


    SYS/BIOS only supports configuring the MMU from the ARM side.

    I hope this helps.

    Alan
  • Thanks!

    Worked like a champ...