I'm using CCSv5.3.0.00090, SYS/BIOS 6.34.2.18, XDCtools 3.24.5.48, Platform ti.platforms.evm6678, target ti.targets.elf.C66
I cannot find where I go to configure the cache MAR register settings. I did a use Cache for both ti.sysbios.famly.c66 and ti.sysbios.hal. When I click on the cache module, I don't get any properties, just a check box that says "Add the cache module to my configuration" which I have checked.
If I use the C64p cache module as just an experment instead, I see the MAR settings but of course the C64p settings don't apply here.
I read another forum post that suggests the MAR settings should be done the Platform file. When I looked at the evm6678 platform file in the plaform wizard, it had nothing in there to set the MAR registers.