Other Parts Discussed in Thread: OMAPL138
Hi All!
This thread was created as a replacement of http://e2e.ti.com/support/embedded/bios/f/355/t/223029.aspx?pi239031349=4. I was told by our local TI distributor that due to the fact that the previous thread was marked as answered it doesn't get enough attention.
CCS 5.1.1.00031
bios_5_42_00_07
ndk_2_20_06_35
ethss_dm648 from ndk_2_0_0. According to TI's advice all "printf" were removed
The project was taken from
ndk_2_0_0\packages\ti\ndk\example\network\helloWorld
This project originally was for CCS 3.3 so I had to convert it to use with CCS 5.1.
I did the following changes in the pfoject:
- an IP address is set statically
- dtask_udp_hello demon and its creation were commented out
- A MainTask thread was created
MainTask sends UDP packets (1000 bytes). The stream is about 150 Mb/s. We also reproduced the problem with 80 Mb/s.
The evaluation module DM648 DVDP is directly connected to a PC. To have more control on the PC we use Free BSD UNIX now. On the PC's side we use hping in flood mode to send packets to the board, netstat to see what is going on on the net and normal ping to test if the board responds (when hping works in flood mode it reports nothing). hping can provide a very big amount of packets and it makes the problem appears faster. Usually we start hping in two threads to use both CPUs of the PC and create maximum traffic. In this case the problem appears within minutes.
There is no application on the PC which would receive data from DM648.
As we understand the situation now, it is necessary that packets were sent in both ways from DM648 and to DM648. The problem happens with both 100 Mb and 1Gb connections.
1. Connect the board and the PC directly with a cable. All modern cards don't require cross cable anymore.
2. Set desired IP addressed on the board and PC.
3. Run the project as it is on the board.
4. Run ping on the PC to watch the state of the board.
5. Start two terminals on the PC and in each run hping –flood –udp 192.168.1.100 (where 192.168.1.100 is the board's IP address)
Hi Victor,
I just wanted to update you. We are able to reproduce this issue and are seeing it on different hardware platforms. We are currently debugging the issue and will let you know as soon as we have something ... thanks again for your patience.