Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hello,
I'm trying to build the SYS/BIOS Hello example program on the ARM9 side of an OMAP-L138. Everything seems to configure (xs), and compile but when it comes time to link I get an undefined symbol, IND_CALL, in an xdc library, auto_init.ae9. If I stub it out, by defining a local function, the build process completes successfully (albeit without the actual function, IND_CALL). My configuration:
general build settings (main):
Output Type: RTSC Application
Family: ARM
Variant: OMAPL138
Device endianess: little
Compiler version: TI v5.1.2
Output format: eabi (ELF)
Runtime support library: <automatic>
general build settings (rtsc):
SYS/BIOS 6.35.1.29
Other Repositories
$(TARGET_CONTENT_BASE)
bios_6_35_01_29
$(BIOS_CG_ROOT)/packages
xdctools_3_24_06_63
compiler: arm_5.1.2
CCS IDE: 5.4.00091
xdc: 3_24_06_63
sys/bios: 6_35_01_29
I can build the same package for the DSP (C6748) side of the OMAP-L138 with no issues. Although searching the DSP's map file no IND_CALL symbol is to be found.
Where is this symbol (IND_CALL) defined? I grepped many libraries without success.
Any suggestions? I built directly from the "Create New CCS Project". Is there a library I'm missing or need to build first?
TIA,
Kevin