Other Parts Discussed in Thread: AM3359, SYSBIOS
Hi,
In a different project our customer needs to run TCP/IP server based on NDK on the AM335x.
But currently they are not able to communicate with the TCP/IP client.
We would like know the answers for the below queries.
1.Is it possible to run a TCP/IP server(based on NDK) on the AM335x ICE2 board?
2.In this case which sys_bios_driver(NDK) should be selected, is it CPSW or ICSS?
3.Which could be the good sample code to refer in this case? is it profinet_slave?
4.We tried to use the profinet_slave sample but we are not able to get the proper communication
(not able to ping and not able to communicate from a TCP/IP client)
Below in the software version used.
SYS/BIOS 6.35.4.50
NDK 2.22.3.20
AM335x_SYS/BIOS_IND_SDK_1.1.0.3
Please let us know if there are any suggestions.
Regards
Prad