Hi,
I am using OMAP 3530. Using DSPLink I am able to load and unload DSP.
I have 2 sample DSP .out files. (DSP1.out and DSP2.out). If i load and unload any one of the out files (either DSP1.out or DSP2.out) continuously each will work fine but when I load DSP1.out then unload and then try to load DSP2.out its causing trouble. Sometimes its showing "DSP MMU Error Fault! MMU_IRQSTATUS = [0x1]. Virtual DSP addr reference that generated the interrupt = [0xff114060]." Error
Both out files try to communicate to ARM through shared memory which currently selected as DSP internal L1DSRAM location. Each out files are of different file size.
Sometimes the linux kernel hangs and the serial console becomes unresponsive. Why is this happening? Please help to fix this problem
Linux kernel version used is - linux-2.6.32-psp03.00.01.06
DSPLink version used is - dsplink_linux_1_65_02_09
regards
Vishnu Prasad