Latest IPC 3.21.00.07 Android applications are not working. Where as old ipc 3.20 Android applications are able to communicate with ipc 3.21 xem4 loaded with late attach feature.
While running lad_dra7xx from Android shell it is throwing an error:
ERROR: Failed to create LAD's working directory!
It is found that changes are made in to
-#define LAD_COMMANDFIFO "/data/local/tmp/LAD/LADCMDS"
-#define LAD_WORKINGDIR "/data/local/tmp/LAD/"
+#define LAD_COMMANDFIFO "/data/lad/LAD/LADCMDS"
+#define LAD_WORKINGDIR "/data/lad/LAD/"
After changing these two lines to old one. lad_dra7xx started running but still messageQApp not able connect to lad server. It throws below error.
Ipc_start: LAD_connect() failed: 4
ProcId (2) must be nonzero and less than 0
Ipc_stop: MessageQ_destroy() failed: -9
Any idea what could be the reason here.
Thanks,
Rabi