Other Parts Discussed in Thread: AM3359
Hello,
We are developing a project using raweth protocal .At the begging , The socket looks running OK.But after some seconds, ti will give EWOULDBLOCK error(35). The faster we tried to receive the packet the sooner the NDK will give the error. But after give the error it can run again for a while, then it will give error again and on and on.
We have also tried to enlarge the PBM size in NDK setting page. It can make the NDK to maintain the running longer. But it wil still fail and give error.
My code is like this:
fdShare(socket_rcv);
/* Retrieve the packets */
bytesrx = (int)recvnc( socket_rcv, (void**)&(pkt_data), 0, &hBuffer );
if(bytesrx >= 0)
{
port->tempinbufs = bytesrx;
memcpy(stack->tempbuf, pkt_data, bytesrx); //give data received
recvncfree(hBuffer);
}
else
{
port->tempinbufs = 0;
memcpy(stack->tempbuf, pkt_data, EC_BUFSIZE); //give 0
//Display the errors
error = fdError();
ConsoleUtilsPrintf("\nError Receiving the packet: %d\n", error);
}
fdClose(socket_rcv);
NDK tick period is 10.(10ms)
receive task period is 100ms
MY SDCtools version: 3.25.0.48
SYSBIOS version: 6.35.1.29
NDK Core versison:2.22.3.20
am3359 ind sdk version : 1.1.0.3