Hi,
Please let me ask some basic questions on the system tick in SYS/BIOS.
We understood the Clock module, by default, uses the ti.sysbios.hal.Timer module to
create a timer to generate the system tick.
1>What is the accuracy of this system tick?
2>And which clock source will be selected by default?
We are using SYS/BIOS(v6.4) with default Clock settings as shown below
the tick period is 1ms, but the Timer ID is mentioned as "ANY",
I would like to know which timer and which clock source will be selected in this case.
In our sample application(on AM3352) using Clock_getTicks() , we found that system tick
is not that accurate. For every 1 second time there is an extra delay of 7ms.
Best Regards
Prad