hi,
I'm using TI-RTOS version "irtos_tivac_2_00_02_36" for TM4C129 controller that run on the DK129, I had a fault during debugging but I don't know how to find the cause of the fault, SO please help.
here is the ROV HWI exception data
Decoded exception,
Decoded,Hard Fault: FORCED: BUSFAULT: PRECISERR.Data Access Error. Address = 0xfff04fbd
Exception context,
$addr,0x20019738
$type,ti.sysbios.family.arm.m3.Hwi.ExcContext
threadType,ti.sysbios.BIOS.ThreadType_Swi
threadHandle,0x2001a27c
threadStack,0x20017898
threadStackSize,8192
r0,0xfff0
r1,0xfff04fbd
r2,0x0
r3,0x20019dc4
r4,0x21a0d
r5,0x1
r6,0xfff04fbd
r7,0xc35
r8,0x2001a300
r9,0x2bdec
r10,0x2bf92
r11,0x0
r12,0x13380300
sp,0x20019810
lr,0x108c7
pc,0xf454
psr,0x1000000
ICSR,0x803
MMFSR,0x0
BFSR,0x82
UFSR,0x0
HFSR,0x40000000
DFSR,0xb
MMAR,0xfff04fbd
BFAR,0xfff04fbd
AFSR,0x0
Exception call stack,
0 ti_sysbios_knl_Clock_workFunc__E() at :0,PC = 0x0000F454 FP = 0x20019810
1 abort() at exit.c:117,PC = 0x0001EC7F FP = 0x20019810
2 ti_sysbios_knl_Task_startup__E() at :0,PC = 0x2001A27C FP = 0x20019818
3 abort() at exit.c:117,PC = 0x0001EC7F FP = 0x20019818
4 ti_sysbios_knl_Task_startup__E() at :0,PC = 0x200199B4 FP = 0x20019820
5 abort() at exit.c:117,PC = 0x0001EC7F FP = 0x20019820
6 <symbol is not available>,PC = 0x00000002 FP = 0x20019828