Other Parts Discussed in Thread: SYSBIOS
Hi
I'm using CCS5 and working with a our own PCB . I'm using the DSP C6655 in our platform. Our platform is based om the EVM C6657 with the same components.
I 'm dealing with several crash issues on runtime when our sw launched from DDR3 and the same sw works fint if the sw is launched from MSM RAM.
From DSP's UART we can have see the error of the kernel hook function:
efr=0x2
nrp=0x8001a4c0
ntsr=0x1820f
ierr=0x0
Error Code:0, File:C:/ti/bios_6_37_01_24/packages/ti/sysbios/knl/Semaphore.c, Line:207
My question is now, can I, som how, get a kind of core dump during after a crash. Then I can load the core dump to debugger and see the call stack ?
BR
Tam Tran
Vestas Wind System