Other Parts Discussed in Thread: SYSBIOS
Hello
I use F28M36xx Control Card and Code Composer version 6.1.0.00104.
I want to use the EPI interface in HB8 mode. The control suite example for EPI is running.
In next step i try to use EPI with TI-RTOS. I tried to modify the TI-RTOS Demo example for EPI:
But It does not work. Where could be the problem?
Regards and waiting for Your response.
ti.sysbios.family.arm.m3.Hwi: line 1087: E_hardFault: FORCED
ti.sysbios.family.arm.m3.Hwi: line 1164: E_busFault: IMPRECISERR: Delayed Bus Fault, exact addr unknown, address: e000ed38
Exception occurred in background thread at PC = 0x0024788a.
Core 0: Exception occurred in ThreadType_Main.
Main name: main(), handle: 0x0.
Main stack base: 0x200010fc.
Main stack size: 0x400.
R0 = 0x400d0000 R8 = 0x00000000
R1 = 0x00000012 R9 = 0x00000000
R2 = 0x00000000 R10 = 0x00000000
R3 = 0x000000f0 R11 = 0x00000000
R4 = 0x00000000 R12 = 0x2000138c
R5 = 0x00000000 SP(R13) = 0x20001478
R6 = 0x00000000 LR(R14) = 0x0024788b
R7 = 0x200014f8 PC(R15) = 0x0024788a
PSR = 0x21000000
ICSR = 0x00400803
MMFSR = 0x00
BFSR = 0x04
UFSR = 0x0000
HFSR = 0x40000000
DFSR = 0x00000000
MMAR = 0xe000ed34
BFAR = 0xe000ed38
AFSR = 0x00000000
Terminating execution...
void SetEPIControl(void)
{
//
// GPIO Port C pins
//
HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL) = GPIO_PCTL_PC4_EPI0S2 |
GPIO_PCTL_PC5_EPI0S3 |
GPIO_PCTL_PC6_EPI0S4 |
GPIO_PCTL_PC7_EPI0S5;
//
// GPIO Port D pins.
//
HWREG(GPIO_PORTD_BASE + GPIO_O_PCTL) = GPIO_PCTL_PD2_EPI0S20 |
GPIO_PCTL_PD3_EPI0S21;
//
// GPIO Port E pins
//
HWREG(GPIO_PORTE_BASE + GPIO_O_PCTL) = GPIO_PCTL_PE0_EPI0S8 |
GPIO_PCTL_PE1_EPI0S9;
//
// GPIO Port F pins
//
HWREG(GPIO_PORTF_BASE + GPIO_O_PCTL) = GPIO_PCTL_PF4_EPI0S12 |
GPIO_PCTL_PF5_EPI0S15;
//
// GPIO Port G pins
//
HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL) = GPIO_PCTL_PG0_EPI0S13 |
GPIO_PCTL_PG1_EPI0S14;
//
// GPIO Port H pins
//
HWREG(GPIO_PORTH_BASE + GPIO_O_PCTL) = GPIO_PCTL_PH0_EPI0S6 |
GPIO_PCTL_PH1_EPI0S7 |
GPIO_PCTL_PH2_EPI0S1 |
GPIO_PCTL_PH3_EPI0S0 |
GPIO_PCTL_PH4_EPI0S10 |
GPIO_PCTL_PH5_EPI0S11;
//
// GPIO Port J pins
//
HWREG(GPIO_PORTJ_BASE + GPIO_O_PCTL) = GPIO_PCTL_PJ0_EPI0S16 |
GPIO_PCTL_PJ1_EPI0S17 |
GPIO_PCTL_PJ2_EPI0S18 |
GPIO_PCTL_PJ3_EPI0S19 |
GPIO_PCTL_PJ4_EPI0S28 |
GPIO_PCTL_PJ5_EPI0S29 |
GPIO_PCTL_PJ6_EPI0S30;
// Enable Clock for EPI & GPIO Ports
// Configure the GPIO setting for the EPI pins.
//SetPortControl();
GPIODirModeSet(GPIO_PORTC_BASE,
(GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7),
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTC_BASE,
(GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7),
GPIO_PIN_TYPE_STD_WPU);
GPIODirModeSet(GPIO_PORTD_BASE,
(GPIO_PIN_2 | GPIO_PIN_3),
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTD_BASE,
(GPIO_PIN_2 | GPIO_PIN_3),
GPIO_PIN_TYPE_STD_WPU);
GPIODirModeSet(GPIO_PORTE_BASE,
(GPIO_PIN_0 | GPIO_PIN_1),
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTE_BASE,
(GPIO_PIN_0 | GPIO_PIN_1),
GPIO_PIN_TYPE_STD_WPU);
GPIODirModeSet(GPIO_PORTF_BASE,
(GPIO_PIN_4 | GPIO_PIN_5),
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTF_BASE,
(GPIO_PIN_4 | GPIO_PIN_5),
GPIO_PIN_TYPE_STD_WPU);
GPIODirModeSet(GPIO_PORTG_BASE,
(GPIO_PIN_0 | GPIO_PIN_1),
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTG_BASE,
(GPIO_PIN_0 | GPIO_PIN_1),
GPIO_PIN_TYPE_STD_WPU);
GPIODirModeSet(GPIO_PORTH_BASE,
(GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 |
GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7),
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTH_BASE,
(GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 |
GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7),
GPIO_PIN_TYPE_STD_WPU);
GPIODirModeSet(GPIO_PORTJ_BASE,
(GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 |
GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6),
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTJ_BASE,
(GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 |
GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6),
GPIO_PIN_TYPE_STD_WPU);
// Set 8 Bit HostBus mode.
EPIModeSet(EPI0_BASE, EPI_MODE_HB8);
EPIDividerSet(EPI0_BASE, 0x1);
// Address & Data are not muxed (ADNOMUX = 0x1).
EPIConfigHB8Set(EPI0_BASE, (EPI_HB8_MODE_ADDEMUX | EPI_HB8_WRWAIT_0 | EPI_HB8_RDWAIT_0), 0);
EPIAddressMapSet(EPI0_BASE, (EPI_ADDR_RAM_SIZE_64KB | EPI_ADDR_RAM_BASE_6) );
}