Other Parts Discussed in Thread: AM3358, AM3356, SYSBIOS, AM3359
Hi,
I have installed the most recent version of CCS (6.1.0.00104). I wish to use it with BeagleBoard Black (Sitara AM3358 processor). I also wanted to use the TI-RTOS for Sitara. According to the documentation it should be installed from the App Center. However it does not appear there. There are Add ons for TI-RTOS for C2000, TivaC, MSP43x and Simplelink, but not for TI-RTOS for Sitara. This video shows that other users do have the TI-RTOS in the App Center https://www.youtube.com/watch?v=iOQisBaDANA. During CCS installation I selected all features. TI-RTOS for Sitara can be installed separately, which I did, but it also installs older version of XDCTools, which I do not want to conflict with the newer version. And because it is not a recommended way, I prefer no to do it this way.
I have also tried it with CCS 6.0.1 with the same result.
Adam