This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error "Illegal priority call to llEnter()" source is priority setting



Can we capture this on E2E? I looked at the only other thread regarding a C2XXX part issue and it really doesn't answer this question.

I finally read the llEnter section (5.2.3) in SPRU523 and it explains the main problem. We were using the SYS/BIOS Task_create() call rather than the NDK task creation call. We were also using a higher priority (12) than the max NDK priority (10) which is documented as a defective way to design your code.

Time to read that section in real detail!!

I have put in a Document Change observation for SPRUEX3 and SPRUHD4 to have the writers add notes to point to the need to use the NDK interfaces is using the NDK.