Hi Sir :
I work on TI AM335x platform, the tools's version are as below.
CCS V6
am335x_sysbios_ind_sdk_1.1.0.8
bios_6_41_04_54
ndk_2_24_01_18
xdctools_3_30_06_67_core
I use SPI example in starterware directory to test SPI interface and I have a question.
Below is the register setting of SPI0.
Below is the time information between two byte.
My question is why the time between two byte is so long?
It takes about 12 us.
Please give me some suggestion.
Best regards,
Marcus