Hello,
I am trying to rebuild library with XDC tools 3_32_00_06 version, the build fails with below error. The same code works with xdctools_3_25_02_70.
XDC 3.32 documentation says "Beginning with the 3.31 release, all embedded targets and platforms have been removed. They are now delivered with middleware products, such as TI-RTOS and Grace, that have dependencies on specific targets and platforms"
How do we add these products into project config?
making package.mak (because of package.bld) ...
js: "./config.bld", line 76: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: can't locate the package 'gnu.targets.arm' along the path: 'D:/ti/bios_6_45_01_29/packages --jobs;D:/ti/xdctools_3_32_00_06_core/packages;../../..;'. Ensure that the package path is set correctly.
gmake[1]: *** No rule to make target `4'. Stop.
xdctools_3_32_00_06_core\gmake.exe: *** [packages/ti/nsp/drv/,4] Error 2
makefile:41: recipe for target 'all' failed
gmake: *** [all] Error 2
Regards,
Prasad