Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuration of zero latency interrupt with respect to a timer

Other Parts Discussed in Thread: SYSBIOS

Hi TI Community,

First of all, I am using a TIVA EK-TM4C1294XL Evaluatioin Board, with TI-RTOS for TivaC product installed (version 2.16.0.08) and Code Composer Studio (v6.1.2.00015).

I am trying to set up a zero latency interrupt that fires repetitively(regularly) after a certain time (currently looking around 2 microseconds) with Timer2A. The interrupt will be used to perform some time critical operation. I have got the following information from pg116 of tn4c1294ncpdt data sheet - 

Vector Number: 39
Interrupt Number: 23
Vector Address or Offset: 0x0000.009C
Description: 16/32-Bit Timer 2A

 I have been searching on the forum for similar topics and I have gone through the below threads:

https://e2e.ti.com/support/embedded/tirtos/f/355/p/508916/1847863#1847863

I was able to follow through the first answer of  to created a HAL level timer interrupt but however not able to follow through with his last answer on creating a zero latency interrupt. I have attached snippets of my code for testing purposes in the empty_project.

Edited .cfg file to include the family specific Timer module.
var Timer = xdc.useModule('ti.sysbios.family.arm.m3.Timer');
__________________________________________________________________
...

#include <ti/sysbios/family/arm/m3/Timer.h>

#include <ti/sysbios/family/arm/m3/Hwi.h>

...
void hwi0_isr(UArg arg){ TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT); GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_3, 0x00); GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_3, 0x0F); } /* * ======== main ======== */ int main(void) { Task_Params taskParams; /* Call board init functions */ Board_initGeneral(); Board_initGPIO(); /* Construct heartBeat Task thread */ ... ... /* Init Timer interrupt and pin P3 for testing */ GPIOPinTypeGPIOOutput(GPIO_PORTP_BASE, GPIO_PIN_3); /* Enable timer peripherial clock */ Timer_Params TimerParams; Timer_Handle myTimer; Hwi_Params hwiParams; Error_Block eb; Error_init(&eb); SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER2); SysCtlPeripheralReset(SYSCTL_PERIPH_TIMER2); while (!SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER2)) { } // initialise zero latency interrupt on timer Timer_Params_init(&TimerParams); TimerParams.period = 10; TimerParams.arg = 1; TimerParams.periodType = Timer_PeriodType_MICROSECS; //can also be in microseconds hwiParams.priority = 0; //zero latency interrupt, priority 0 TimerParams.hwiParams = &hwiParams; //Termination error when timerID = 0 and Timer_ANY, I tried 1,2, 23(interrupt number of Timer2A), 39(vector number of Timer2A). myTimer = Timer_create(*I am not too sure about this field, see above comment*, hwi0_isr, &TimerParams, &eb); if (myTimer == NULL) { System_abort("Timer create failed"); } /* Start BIOS */ BIOS_start(); return (0); }

My understanding is that the following line is configuring the interrupt to have a zero latency priority and the struct "hwiParams" is later passed into "TimerParams" as the config of Timer_create.

    hwiParams.priority = 0;       //zero latency interrupt, priority 0

I am getting the following error on launch after debug (no compile error as well) when I set TimerId to be 2 for Timer_create.

- ti.sysbios.family.arm.m3.Timer: line 162: E_invalidTimer: Invalid Timer Id 2

- Timer create failed

Thanks in advance for your help!

Gabriel

p.s I have also gone through software-dl.ti.com/.../Hwi.html

  • Gabriel,

    ti.sysbios.family.arm.m3.Timer is the SysTick timer in the NVIC.  There is only one physical timer instance available, so you should only pass an “id” of zero or Timer_ANY to Timer_create(). (This first parameter is a zero-based numeric index of available timers, and there is only one instance of SysTick.)

    When you specified 0 or Timer_ANY what error did you get?  I’m guessing the SysTick might already be in use in your application.  If you attach your application’s .cfg we can see.

    On this device there are also 8 general purpose timers (GPTM).  The Timer2A that you are referencing is half of one of these general purpose timers.  To use that timer:

    1) use ti.sysbios.family.arm.lm4.Timer instead of ti.sysbios.family.arm.m3.Timer

    2) specify timer instance “2” in the create call:
        Timer_create(2, hwi0_isr, &TimerParams, &eb);


    Regards,
    Scott