This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Program works correctly in Debug mode only

Other Parts Discussed in Thread: CC1310

Hi,

Working on CC1310, I have a program that works just fine when executed from within the debugger. However, the moment I stop the debugger, or trying to execute the code without the debugger, the program does not work.

I found another thread that suggested disabling 'SemiHosting' if using GNU compiler. However in my case I am using ARM compiler & Linker, so what do I need to do to have my debug release work correctly even when not connected to a debugger?


Basically I have a clock object that is supposed to call a function every 1 second. When using the debugger everything works as expected. However when I power on the board without the debugger, strangely enough the clock function gets called only once and then never.

Thanks


This is my main code

/*
 * Copyright (c) 2015-2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ======== empty_min.c ========
 */
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Log.h>
#include <xdc/cfg/global.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Swi.h>

/* TI-RTOS Header files */
#include <ti/drivers/PIN.h>
#include <ti/drivers/ADC.h>

/* Easylink header files */
#include "easylink/EasyLink.h"

/* Board Header files */
#include "Board.h"


PIN_Handle ledPinHandle = NULL;

PIN_Config ledPinTable[] = {
    Board_LED1     | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    Board_LED2     | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
	Board_LED3     | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
	Board_LED4     | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    PIN_TERMINATE
};

typedef enum OPERATION_result
{
	OPERATION_SUCCESS = 0,
	OPERATION_FAIL = -1
}OPERATION_result_t;


void LED_dance(void);
OPERATION_result_t RF_send(UInt16 data);
OPERATION_result_t ADC_get(UInt16 *res);

int main(void)
{
	//board init functions
    Board_initGeneral();
    Board_initADC();

    PIN_State ledPinState;

    ledPinHandle = PIN_open(&ledPinState, ledPinTable);
    if(!ledPinHandle) {
        Log_info0("Error initializing board LED pins");
    }

    LED_dance();

    /* Start BIOS */
    BIOS_start();

    return (0);
}

//every 2 second swi to
//1. get ALS ADC reading
//2. send the ADC reading through RF
void clock_adc_rf_fn(UArg a0)
{
	//post the RF swi
	Swi_post(swi_simplelink_rf);
}

void LED_dance(void)
{
	UInt32 i = 0;
	PIN_setOutputValue(ledPinHandle, Board_LED1, 1);

	i = 3000000;
	while(i != 0)
	{
		i--;
	}
	PIN_setOutputValue(ledPinHandle, Board_LED2, 1);

	i = 3000000;
	while(i != 0)
	{
		i--;
	}
	PIN_setOutputValue(ledPinHandle, Board_LED3, 1);

	i = 3000000;
	while(i != 0)
	{
		i--;
	}
	PIN_setOutputValue(ledPinHandle, Board_LED4, 1);

	i = 3000000;
	while(i != 0)
	{
		i--;
	}
	PIN_setOutputValue(ledPinHandle, Board_LED1, 0);
	PIN_setOutputValue(ledPinHandle, Board_LED2, 0);
	PIN_setOutputValue(ledPinHandle, Board_LED3, 0);
	PIN_setOutputValue(ledPinHandle, Board_LED4, 0);
}


//send the supplied 12 bit ADC data through RF
OPERATION_result_t RF_send(UInt16 data)
{
	EasyLink_TxPacket txpacket = {{0}, 0 , 0, {0}};
	txpacket.dstAddr[0] = 0xaa;
	txpacket.len = 1;
	txpacket.absTime = 0;
	txpacket.payload[0] = (UInt8)data;

	EasyLink_Status result = EasyLink_transmit(&txpacket);

	if(result == EasyLink_Status_Success)
	{
		//toggle blue LED
		UInt32 i = 0;
		PIN_setOutputValue(ledPinHandle, Board_LED4, 1);

		i = 300000;
		while(i != 0)
		{
			i--;
		}
		PIN_setOutputValue(ledPinHandle, Board_LED4, 0);

		return OPERATION_SUCCESS;
	}
	return OPERATION_FAIL;
}

OPERATION_result_t ADC_get(UInt16 *res)
{
	ADC_Handle   adc;
	ADC_Params   params;
	UInt16 result;
	UInt16 adcValue0;

	ADC_Params_init(&params);
	adc = ADC_open(Board_ADC0, &params);

	if (adc == NULL)
	{
		Log_info0("Error initializing ADC channel 0\n");
		return OPERATION_FAIL;
	}
	else
	{
		Log_info0("ADC channel 0 initialized\n");
	}

	/* Blocking mode conversion */
	result = ADC_convert(adc, &adcValue0);

	if (result == ADC_STATUS_SUCCESS)
	{
		Log_info1("ADC channel 0 convert result: [%u]", adcValue0);
		*res = adcValue0;
		ADC_close(adc);
		return OPERATION_SUCCESS;
	}
	else
	{
		System_printf("ADC channel 0 convert failed\n");
		ADC_close(adc);
		return OPERATION_FAIL;
	}
	return OPERATION_FAIL;
}

void task_easylink_init_fn(UArg a0, UArg a1)
{
	//init easylink module
	if(EasyLink_init(EasyLink_Phy_50kbps2gfsk) != EasyLink_Status_Success)
	{
		Log_info0("error starting easylink");
		PIN_setOutputValue(ledPinHandle, Board_LED1, 1);
	}
	Log_info0("easylink init complete");
	EasyLink_setFrequency(868000000);
	EasyLink_setRfPwr(12);
}

void swi_simplelink_rf_fn(UArg a0, UArg a1)
{
	UInt32 i = 0;

	Log_info0("clock adc + rf function");

	PIN_setOutputValue(ledPinHandle, Board_LED2, 1);

	//get ADC data
	UInt16 adc_val;
	if(ADC_get(&adc_val) == OPERATION_SUCCESS)
	{
		Log_info1("ADC reading [%u]", adc_val);
		PIN_setOutputValue(ledPinHandle, Board_LED1, 0);

		//send ADC data through RF
		if(RF_send(adc_val) == OPERATION_SUCCESS)
		{
			Log_info1("sent value [%u] through RF link", adc_val);
			PIN_setOutputValue(ledPinHandle, Board_LED1, 0);
		}
		else
		{
			//set error led
			PIN_setOutputValue(ledPinHandle, Board_LED1, 1);
		}
	}
	else
	{
		//set error led
		PIN_setOutputValue(ledPinHandle, Board_LED1, 1);
	}

	//put some delay so that can see led2 tick
	i = 1000000;
	while(i != 0)
	{
		i--;
	}
	PIN_setOutputValue(ledPinHandle, Board_LED2, 0);
}

This is my configuration file

/* ================ Boot configuration ================ */
var Boot = xdc.useModule('ti.sysbios.family.arm.cc26xx.Boot');
/*
 * This module contains family specific Boot APIs and configuration settings.
 * See the SYS/BIOS API guide for more information.
 */



/* ================ Clock configuration ================ */
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup');
var Timer = xdc.useModule('ti.sysbios.hal.Timer');
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
/*
 * When using Power and calibrateRCOSC is set to true, this should be set to 10.
 * The timer used by the Clock module supports TickMode_DYNAMIC. This enables us
 * to set the tick period to 10 us without generating the overhead of additional
 * interrupts.
 *
 * Note: The calibrateRCOSC parameter is set within the Power configuration
 *     structure in the "Board.c" file.
 */
Clock.tickPeriod = 10;



/* ================ Defaults (module) configuration ================ */
var Defaults = xdc.useModule('xdc.runtime.Defaults');
/*
 * A flag to allow module names to be loaded on the target. Module name
 * strings are placed in the .const section for debugging purposes.
 *
 * Pick one:
 *  - true (default)
 *      Setting this parameter to true will include name strings in the .const
 *      section so that Errors and Asserts are easier to debug.
 *  - false
 *      Setting this parameter to false will reduce footprint in the .const
 *      section. As a result, Error and Assert messages will contain an
 *      "unknown module" prefix instead of the actual module name.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Defaults.common$.namedModule = true;
Defaults.common$.namedModule = false;



/* ================ Error configuration ================ */
var Error = xdc.useModule('xdc.runtime.Error');
/*
 * This function is called to handle all raised errors, but unlike
 * Error.raiseHook, this function is responsible for completely handling the
 * error with an appropriately initialized Error_Block.
 *
 * Pick one:
 *  - Error.policyDefault (default)
 *      Calls Error.raiseHook with an initialized Error_Block structure and logs
 *      the error using the module's logger.
 *  - Error.policySpin
 *      Simple alternative that traps on a while(1) loop for minimized target
 *      footprint.
 *      Using Error.policySpin, the Error.raiseHook will NOT called.
 */
//Error.policyFxn = Error.policyDefault;
Error.policyFxn = Error.policySpin;

/*
 * If Error.policyFxn is set to Error.policyDefault, this function is called
 * whenever an error is raised by the Error module.
 *
 * Pick one:
 *  - Error.print (default)
 *      Errors are formatted and output via System_printf() for easier
 *      debugging.
 *  - null
 *      Errors are not formatted or logged. This option reduces code footprint.
 *  - non-null function
 *      Errors invoke custom user function. See the Error module documentation
 *      for more details.
 */
//Error.raiseHook = Error.print;
Error.raiseHook = null;
//Error.raiseHook = "&myErrorFxn";

/*
 * If Error.policyFxn is set to Error.policyDefault, this option applies to the
 * maximum number of times the Error.raiseHook function can be recursively
 * invoked. This option limits the possibility of an infinite recursion that
 * could lead to a stack overflow.
 * The default value is 16.
 */
Error.maxDepth = 2;



/* ================ Hwi configuration ================ */
var halHwi = xdc.useModule('ti.sysbios.hal.Hwi');
var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
/*
 * Checks for Hwi (system) stack overruns while in the Idle loop.
 *
 * Pick one:
 *  - true (default)
 *      Checks the top word for system stack overflows during the idle loop and
 *      raises an Error if one is detected.
 *  - false
 *      Disabling the runtime check improves runtime performance and yields a
 *      reduced flash footprint.
 */
//halHwi.checkStackFlag = true;
halHwi.checkStackFlag = false;

/*
 * The following options alter the system's behavior when a hardware exception
 * is detected.
 *
 * Pick one:
 *  - Hwi.enableException = true
 *      This option causes the default m3Hwi.excHandlerFunc function to fully
 *      decode an exception and dump the registers to the system console.
 *      This option raises errors in the Error module and displays the
 *      exception in ROV.
 *  - Hwi.enableException = false
 *      This option reduces code footprint by not decoding or printing the
 *      exception to the system console.
 *      It however still raises errors in the Error module and displays the
 *      exception in ROV.
 *  - Hwi.excHandlerFunc = null
 *      This is the most aggressive option for code footprint savings; but it
 *      can difficult to debug exceptions. It reduces flash footprint by
 *      plugging in a default while(1) trap when exception occur. This option
 *      does not raise an error with the Error module.
 */
//m3Hwi.enableException = true;
//m3Hwi.enableException = false;
m3Hwi.excHandlerFunc = null;

/*
 * Enable hardware exception generation when dividing by zero.
 *
 * Pick one:
 *  - 0 (default)
 *      Disables hardware exceptions when dividing by zero
 *  - 1
 *      Enables hardware exceptions when dividing by zero
 */
m3Hwi.nvicCCR.DIV_0_TRP = 0;
//m3Hwi.nvicCCR.DIV_0_TRP = 1;

/*
 * Enable hardware exception generation for invalid data alignment.
 *
 * Pick one:
 *  - 0 (default)
 *      Disables hardware exceptions for data alignment
 *  - 1
 *      Enables hardware exceptions for data alignment
 */
m3Hwi.nvicCCR.UNALIGN_TRP = 0;
//m3Hwi.nvicCCR.UNALIGN_TRP = 1;

/*
 * Assign an address for the reset vector.
 *
 * Default is 0x0, which is the start of Flash. Ordinarily this setting should
 * not be changed.
 */
m3Hwi.resetVectorAddress = 0x0;

/*
 * Assign an address for the vector table in RAM.
 *
 * The default is the start of RAM. This table is placed in RAM so interrupts
 * can be added at runtime.
 *
 * Note: To change, verify address in the device specific datasheets'
 *     memory map.
 */
m3Hwi.vectorTableAddress = 0x20000000;
/*
 * The Idle module is used to specify a list of functions to be called when no
 * other tasks are running in the system.
 *
 * Functions added here will be run continuously within the idle task.
 *
 * Function signature:
 *     Void func(Void);
 */
//Idle.addFunc("&myIdleFunc");



/* ================ Kernel (SYS/BIOS) configuration ================ */
var BIOS = xdc.useModule('ti.sysbios.BIOS');
/*
 * Enable asserts in the BIOS library.
 *
 * Pick one:
 *  - true (default)
 *      Enables asserts for debugging purposes.
 *  - false
 *      Disables asserts for a reduced code footprint and better performance.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//BIOS.assertsEnabled = true;
BIOS.assertsEnabled = false;

/*
 * Specify default heap size for BIOS.
 */
BIOS.heapSize = 1024;

/*
 * Specify default CPU Frequency.
 */
BIOS.cpuFreq.lo = 48000000;

/*
 * A flag to determine if xdc.runtime sources are to be included in a custom
 * built BIOS library.
 *
 * Pick one:
 *  - false (default)
 *      The pre-built xdc.runtime library is provided by the respective target
 *      used to build the application.
 *  - true
 *      xdc.runtime library sources are to be included in the custom BIOS
 *      library. This option yields the most efficient library in both code
 *      footprint and runtime performance.
 */
//BIOS.includeXdcRuntime = false;
BIOS.includeXdcRuntime = true;

/*
 * The SYS/BIOS runtime is provided in the form of a library that is linked
 * with the application. Several forms of this library are provided with the
 * SYS/BIOS product.
 *
 * Pick one:
 *   - BIOS.LibType_Custom
 *      Custom built library that is highly optimized for code footprint and
 *      runtime performance.
 *   - BIOS.LibType_Debug
 *      Custom built library that is non-optimized that can be used to
 *      single-step through APIs with a debugger.
 *
 */
BIOS.libType = BIOS.LibType_Debug;
//BIOS.libType = BIOS.LibType_Debug;

/*
 * Runtime instance creation enable flag.
 *
 * Pick one:
 *   - true (default)
 *      Allows Mod_create() and Mod_delete() to be called at runtime which
 *      requires a default heap for dynamic memory allocation.
 *   - false
 *      Reduces code footprint by disallowing Mod_create() and Mod_delete() to
 *      be called at runtime. Object instances are constructed via
 *      Mod_construct() and destructed via Mod_destruct().
 *
 *  When using BIOS in ROM:
 *      This option must be set to true.
 */
BIOS.runtimeCreatesEnabled = true;
//BIOS.runtimeCreatesEnabled = false;

/*
 * Enable logs in the BIOS library.
 *
 * Pick one:
 *  - true (default)
 *      Enables logs for debugging purposes.
 *  - false
 *      Disables logging for reduced code footprint and improved runtime
 *      performance.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//BIOS.logsEnabled = true;
BIOS.logsEnabled = false;



/* ================ Memory configuration ================ */
var Memory = xdc.useModule('xdc.runtime.Memory');
/*
 * The Memory module itself simply provides a common interface for any
 * variety of system and application specific memory management policies
 * implemented by the IHeap modules(Ex. HeapMem, HeapBuf).
 */



/* ================ Program configuration ================ */
/*
 *  Program.stack is ignored with IAR. Use the project options in
 *  IAR Embedded Workbench to alter the system stack size.
 */
if (!Program.build.target.$name.match(/iar/)) {
    /*
     *  Reducing the system stack size (used by ISRs and Swis) to reduce
     *  RAM usage.
     */
Program.stack = 1024;
}



/*
 * Uncomment to enable Semihosting for GNU targets to print to the CCS console.
 * Please read the following TIRTOS Wiki page for more information on Semihosting:
 * http://processors.wiki.ti.com/index.php/TI-RTOS_Examples_SemiHosting
 */

if (Program.build.target.$name.match(/gnu/)) {
    //var SemiHost = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport');
}

/* ================ ROM configuration ================ */
/*
 * To use BIOS in flash, comment out the code block below.
 */
var ROM = xdc.useModule('ti.sysbios.rom.ROM');
if (Program.cpu.deviceName.match(/CC26/)) {
    ROM.romName = ROM.CC2650;
}
else if (Program.cpu.deviceName.match(/CC13/)) {
    ROM.romName = ROM.CC1350;
}



/* ================ Semaphore configuration ================ */
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
/*
 * Enables global support for Task priority pend queuing.
 *
 * Pick one:
 *  - true (default)
 *      This allows pending tasks to be serviced based on their task priority.
 *  - false
 *      Pending tasks are services based on first in, first out basis.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Semaphore.supportsPriority = true;
Semaphore.supportsPriority = false;

/*
 * Allows for the implicit posting of events through the semaphore,
 * disable for additional code saving.
 *
 * Pick one:
 *  - true
 *      This allows the Semaphore module to post semaphores and events
 *      simultaneously.
 *  - false (default)
 *      Events must be explicitly posted to unblock tasks.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Semaphore.supportsEvents = true;
Semaphore.supportsEvents = false;



/* ================ System configuration ================ */
var System = xdc.useModule('xdc.runtime.System');
/*
 * The Abort handler is called when the system exits abnormally.
 *
 * Pick one:
 *  - System.abortStd (default)
 *      Call the ANSI C Standard 'abort()' to terminate the application.
 *  - System.abortSpin
 *      A lightweight abort function that loops indefinitely in a while(1) trap
 *      function.
 *  - A custom abort handler
 *      A user-defined function. See the System module documentation for
 *      details.
 */
//System.abortFxn = System.abortStd;
System.abortFxn = System.abortSpin;
//System.abortFxn = "&myAbortSystem";

/*
 * The Exit handler is called when the system exits normally.
 *
 * Pick one:
 *  - System.exitStd (default)
 *      Call the ANSI C Standard 'exit()' to terminate the application.
 *  - System.exitSpin
 *      A lightweight exit function that loops indefinitely in a while(1) trap
 *      function.
 *  - A custom exit function
 *      A user-defined function. See the System module documentation for
 *      details.
 */
//System.exitFxn = System.exitStd;
System.exitFxn = System.exitSpin;
//System.exitFxn = "&myExitSystem";

/*
 * Minimize exit handler array in the System module. The System module includes
 * an array of functions that are registered with System_atexit() which is
 * called by System_exit(). The default value is 8.
 */
System.maxAtexitHandlers = 0;

/*
 * The System.SupportProxy defines a low-level implementation of System
 * functions such as System_printf(), System_flush(), etc.
 *
 * Pick one pair:
 *  - SysMin
 *      This module maintains an internal configurable circular buffer that
 *      stores the output until System_flush() is called.
 *      The size of the circular buffer is set via SysMin.bufSize.
 *  - SysCallback
 *      SysCallback allows for user-defined implementations for System APIs.
 *      The SysCallback support proxy has a smaller code footprint and can be
 *      used to supply custom System_printf services.
 *      The default SysCallback functions point to stub functions. See the
 *      SysCallback module's documentation.
 */
//var SysMin = xdc.useModule('xdc.runtime.SysMin');
//SysMin.bufSize = 128;
//System.SupportProxy = SysMin;
var SysCallback = xdc.useModule('xdc.runtime.SysCallback');
System.SupportProxy = SysCallback;
//SysCallback.abortFxn = "&myUserAbort";
//SysCallback.exitFxn  = "&myUserExit";
//SysCallback.flushFxn = "&myUserFlush";
//SysCallback.putchFxn = "&myUserPutch";
//SysCallback.readyFxn = "&myUserReady";



/* ================ Task configuration ================ */
var Task = xdc.useModule('ti.sysbios.knl.Task');
/*
 * Check task stacks for overflow conditions.
 *
 * Pick one:
 *  - true (default)
 *      Enables runtime checks for task stack overflow conditions during
 *      context switching ("from" and "to")
 *  - false
 *      Disables runtime checks for task stack overflow conditions.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Task.checkStackFlag = true;
Task.checkStackFlag = false;

/*
 * Set the default task stack size when creating tasks.
 *
 * The default is dependent on the device being used. Reducing the default stack
 * size yields greater memory savings.
 */
Task.defaultStackSize = 1024;

/*
 * Enables the idle task.
 *
 * Pick one:
 *  - true (default)
 *      Creates a task with priority of 0 which calls idle hook functions. This
 *      option must be set to true to gain power savings provided by the Power
 *      module.
 *  - false
 *      No idle task is created. This option consumes less memory as no
 *      additional default task stack is needed.
 *      To gain power savings by the Power module without having the idle task,
 *      add Idle.run as the Task.allBlockedFunc.
 */
Task.enableIdleTask = true;
//Task.enableIdleTask = false;
//Task.allBlockedFunc = Idle.run;

/*
 * If Task.enableIdleTask is set to true, this option sets the idle task's
 * stack size.
 *
 * Reducing the idle stack size yields greater memory savings.
 */
Task.idleTaskStackSize = 512;

/*
 * Reduce the number of task priorities.
 * The default is 16.
 * Decreasing the number of task priorities yield memory savings.
 */
Task.numPriorities = 4;



/* ================ Text configuration ================ */
var Text = xdc.useModule('xdc.runtime.Text');
/*
 * These strings are placed in the .const section. Setting this parameter to
 * false will save space in the .const section. Error, Assert and Log messages
 * will print raw ids and args instead of a formatted message.
 *
 * Pick one:
 *  - true (default)
 *      This option loads test string into the .const for easier debugging.
 *  - false
 *      This option reduces the .const footprint.
 */
//Text.isLoaded = true;
Text.isLoaded = false;



/* ================ Types configuration ================ */
var Types = xdc.useModule('xdc.runtime.Types');
/*
 * This module defines basic constants and types used throughout the
 * xdc.runtime package.
 */



/* ================ TI-RTOS middleware configuration ================ */
var mwConfig = xdc.useModule('ti.mw.Config');
/*
 * Include TI-RTOS middleware libraries
 */



/* ================ TI-RTOS drivers' configuration ================ */
var driversConfig = xdc.useModule('ti.drivers.Config');
/*
 * Include TI-RTOS drivers
 *
 * Pick one:
 *  - driversConfig.LibType_NonInstrumented (default)
 *      Use TI-RTOS drivers library optimized for footprint and performance
 *      without asserts or logs.
 *  - driversConfig.LibType_Instrumented
 *      Use TI-RTOS drivers library for debugging with asserts and logs enabled.
 */
driversConfig.libType = driversConfig.LibType_NonInstrumented;
Clock.tickMode = Clock.TickMode_DYNAMIC;
var clock0Params = new Clock.Params();
clock0Params.instance.name = "clock_adc_rf";
clock0Params.period = 100000;
clock0Params.startFlag = true;
clock0Params.arg = null;
Program.global.clock_adc_rf = Clock.create("&clock_adc_rf_fn", 100000, clock0Params);
Clock.timerId = -1;
Clock.swiPriority = 5;
var task0Params = new Task.Params();
task0Params.instance.name = "tast_easylink_init";
task0Params.stackSize = 1024;
Program.global.tast_easylink_init = Task.create("&task_easylink_init_fn", task0Params);
BIOS.customCCOpts = "--endian=little -mv7M3 --abi=eabi -q -ms --opt_for_speed=0  --program_level_compile -g";
var swi0Params = new Swi.Params();
swi0Params.instance.name = "swi_simplelink_rf";
swi0Params.priority = 3;
Program.global.swi_simplelink_rf = Swi.create("&swi_simplelink_rf_fn", swi0Params);

As you can see, I also tried posting an swi from the clock function rather than doing all the execution from within the clock function. The result is the same (LED2 and LED4 blink once ie. the swi function is called once). After that nothing.

  • We'll need more information about your problem:

    What version of SYS/BIOS and TI-RTOS are you using?

    Is it possible to see some code how you create and start the clock?

    How do you know that the clock function never gets called again when the debugger is not connected?
  • Information added in the main post. Upon further investigation, I found out that the function EasyLink_transmit is the one responsible for this behaviour. Temporarily commenting it out or using EasyLink_transmitAsync gets rid of this issue. Not sure why though
  • Hi Ankit,

    EasyLink_transmit is a blocking call that waits until the transmission is complete before returning. EasyLink_transmitAsync is an asynchronous version of the transmit call, which just sends the data to be transmitted over RF and returns almost immediately afterwards. Generally speaking, you want your Swi functions (or any interrupt function for that matter) to occur as quickly as possible, since they operate at the interrupt context, which is a higher priority than regular Tasks. The longer a Swi takes, the more opportunity there is for you to miss timing deadlines and not let other Tasks run. For most cases, you do NOT want to block in an interrupt context. It can greatly increase how long the Swi function takes, which leads to some of the issues stated previously. I'd also advise against having delays in the Swi function for the same reasons.

    Regards,

    Gilbert

  • Hi Gilbert,

    Thank you for the detailed explanation.

    However I still fail to understand how the blocking version of a function call would prevent my code from executing in a non debug environment.

    Thanks.
  • Hi Ankit,

    It is an odd issue for sure. I know the debugger does add some overhead to the project. More overhead is added during single-stepping and breakpoint usage, since it involves stopping the processor and can mess with the timing tasks or interrupts are supposed to run (especially during single-stepping). It also does not help that blocking in an interrupt context is not well defined for our RTOS (another reason to avoid it). I'm not entirely certain about your setup, but it is possible that the debugger's overhead added just enough delay for it to work properly.

    Regards,
    Gilbert