Part Number: CC2640
Tool/software: TI-RTOS
I am using the TI-SDK ble_sdk_2_02_01_18 release on CC2640.
When I tried to convert a float into string for print out, the system will crash.
I created the test code as below, function will never return.
However, if I use "%6d" instead, function will return just fine.
I had already checked suggestion which
- #include <stdio.h> is there
- increase the stack size from 700 to 1000
void test1(float value)
{
char buf[50];
sprintf(buf, "%.4f", value);
// sprintf(buf, "%f", value);
// sprintf(buf, "%6d", (int)value);
System_printf(buf);
System_printf("\n");System_flush();
}
Thanks for advice and suggestions