Part Number: TDC1000-TDC7200EVM
Hello,
1) My metal tank is 1m height and <100 cm width is it required that i should mount two piezo transducers to the tank ??? so that i can get accurate measurement ,should i require two or more than two ???if two is the case then i shoud use two tdc1000-7200 evm modules??
2) Now ,I want to connect sim 900 (gprs module) for my set up for providing internet so that i can able to fetch my data and send the data to my dash board via cloud.Is this possible with tdc 1000-7200 module????
Thanks ,
Murali.