All,
We used to use two IP addresses in our CE6 system (one internal and one external). Now, we'd like to use the same with WEC7 (CE7) and with exactly the same settings the second IP address is ignored.
Our design is very similar to the EVM board - we use the SMSC adapter and we set two IP addresses this way:
[HKEY_LOCAL_MACHINE\Comm\SMSC91181\Parms\TcpIp]
"EnableDHCP"=dword:0
"IpAddress"=multi_sz:"192.168.0.22","192.168.1.3"
"Subnetmask"=multi_sz:"255.255.255.0","255.255.255.0"
"DefaultGateway"="192.168.1.1"
"UseZeroBroadcast"=dword:0
With exactly the same hardware, it doesn't work for CE7.
The "ipconfig /all" for CE6 shows both IP addresses, for CE7 only the first one is displayed (and used).
Please let me know if you have any thoughts on this.
Thank you!
Best regards,
Zack